Part Number: TPS6521815 Hi, I'm Taka.
I use the PWR_EN pin for power up.
The PWR_EN pin has a deglitch circuit and the deglitch time is typ 10ms.
What is the maximum and minimum deglitch time?
Part Number: TPS6521815
Hi, I search for PMIC for Vatics SiP module I5S series.
The Vatics part number is I5502S.
Inpu t voltage of desired PMIC is 4.9-5.1V
Outputs of desired PMIC are total number of 5: 1.05V/1.8A max 1.2V/1.8A max 1.8V/1.8A…
Part Number: TPS6521815 Hi,
I have a question about "Note" in datasheet P45, 8.5.1 Programming Power-Up Default Values.
<Note>Only bits marked with (E2) in the register map have EEPROM programmable power-up default settings. All other bits keep the…
Part Number: TPS6521815 Hi TI,
I use the another MUC to implement programming TPS6521815 by I2C. There are some question I need to check.
1. How to elevate INT_LDO from 2.5V to 3.6V?
2. If I can elevate INT_LDO, next the address 0x26 needs to program…
Part Number: TPS6521815 Other Parts Discussed in Thread: TPS65218 , TPS6521855 Hi Brenda,
It is about PMIC TPS6521815 In system Programming.
The MAIN question is: Is it possible to program/re-program the TPS6521815 with PWR_EN set LOW?
For our…
Part Number: TPS6521815 Other Parts Discussed in Thread: TIDA-00478 TIDA-00478 uses TPS6521815 for supplying power to Zynq 7010. In our system, a DDR3 RAM is used along with Zynq 7020. What is your recommendation to generate the 0.75V reference voltage…
Part Number: TPS6521815 Other Parts Discussed in Thread: TPS65023 Hello, Is there a smaller version of the TPS6521815 available by chance? We need a PMIC which has:
(1) Buck/Boost
(1-2) Buck
(2-4) LDOs
This part is a little larger than what…
Part Number: TPS6521815 Other Parts Discussed in Thread: TPS65218 We have checked the specification of this part and it fits our processor requirement.
I am trying to find solutions of below queries and need help.
(1)In which kind of applications…
Part Number: TPS6521815 Other Parts Discussed in Thread: TPS65217 , TPS65216 , TPS65218 , TPS650861 Hi -
I'm looking for a PMIC that has:
at least 3 Buck outputs with voltage ranges from 0.6V to 3.3V, output currents in the range of 2-3 Amps.
…