Part Number: TPS6521825
Hello TI Forum,
Can anyone tell me what is the maximum input voltage for digital input pins on the TPS6521825? The datasheet doesn't say. Specifically, I want to know the max input voltage for PFI, PB, PWR_EN, SDA, SCL, GPIO1…
Part Number: TPS65218D0 Other Parts Discussed in Thread: AM3352 , TPS6521825 Tool/software: Hello,
This question is related to the one I asked previously that got resolved by changing the PMIC reference to TPS65218D0.
However, once I assembled the…
Part Number: TIDA-050038 Other Parts Discussed in Thread: TPS6521825 , Hi team,
My customer is looking for PMIC for i.MX 8M mini.
TIDA-050038 has two PMICs, TPS6521825+LP873347.
Is there any device that can power i.MX 8M mini with only one device…
Please refer to this Tech Note:
Powering the NXP i.MX 8M Mini with the TPS6521825 and LP873347 PMICs
We are updating part number from TPS65218D0 to TPS6521825, which is pre-programmed to work with LP873347.
This board has been built and we are…
Koyo Asaishi said: Does LP873347 have a OTP setting register for AM570x? No, the LP873347 has OTP settings for NXP i.MX 8M Mini.
Please refer to the LP873347 Technical Reference Manual to see the OTP settings of this device variant and the Powering…
Part Number: TPS65218D0 Other Parts Discussed in Thread: TPS65218 , TPS6521815 , TPS6521825 , TPS6521835 , TPS6521845
Dear team,
What is big difference between TPS65218D0/15/25/35/45? These PMICs seems to have same sequence and same default output…
Hi Daniel,
Thanks for the reply. I did some more digging into this issue and discovered the answer to my initial question: a short circuit is not a short circuit when it is caused by insufficient voltage on the input to the LDO. As for why there is…
Michael,
This makes perfect sense to me :-)
TPS65218 devices will always have CHIPID = 0x03 (the '3' indicates silicon Rev. B1, NRND)
TPS65218D0 devices will always have CHIPID = 0x05 (the '5' indicates silicon Rev. D0, which is stated in the…
Part Number: LP8733 Other Parts Discussed in Thread: TPS6521825 Hello,
I'm interested in using the LP873347 in a circuit I am making, and I have a question about the power-up and power-down sequence this chip goes through. I understand that if EN goes…
Part Number: TPS65218 Other Parts Discussed in Thread: , , , , TPS65910 , TPS650250 , TPS65217 , IPG-UI , USB2ANY I am designing a board with the Am335x and the TPS65218xx. It is pretty bare bones so I don't need RTC, DCDC5 or DCDC6, but I am running…