Part Number: TPS65218 Other Parts Discussed in Thread: AM3354 Hello,
I was directed to the E2E forum by TI customer support to request a schematic review for the TPS65218D0 PMIC.
The PMIC is used in a custom AM3354 System-on-Module (SoM) design to…
Part Number: TPS65218D0
Please check the attached document. After startup, the output periodically turns OFF and the device repeatedly restarts. What could be the cause?
If there's one thing that concerns me, it's that the PGOOD_PMIC (PS4-8pin) output…
Part Number: TPS65218D0 Tool/software: It may be useful to perform a full power cycle of the AM335x initiated via software control of the TPS65218D0 PMIC from the AM335x using the I2C interface. Is this possible in the TPS65218D0?
I see the push button…
Part Number: TPS65218D0 Other Parts Discussed in Thread: TPS6521815 Hi Team,
I am updating my design to include power backup in case the 5V power rail (connected to our PMIC input in the attached schematics) is absent.
I have a question: If I add…
Part Number: TPS65218D0 Other Parts Discussed in Thread: AM4378 Tool/software: Hi all,
I asked in a related thread before.
The output of DCDC4 drops at the timing of the red line in the attached file, and I confirmed that it does not start normally…
Part Number: TPS65218D0 We need two details about the part TPS65218D0.
We are planning to use 3.3V rail as input voltage for all DCDC Step-Down Converters. So Can we generate 3.3V output with the input of 3.3V in any of DCDC convertors ?
…
Part Number: TPS65218D0 Tool/software: As shown in the image below, the total capacitance of the bypass capacitors connected in parallel to the DCDC4 line is 216uF※ Cout 10uF included .
All are multilayer ceramic capacitors (0603~3216m).
Will this…
Part Number: TPS65218D0 Other Parts Discussed in Thread: AM3351 Tool/software: The image below shows "RTC_PMIC_EN" coming from somewhere to the PWR_EN of the PMIC (presumably pin 46). In our current design we have the PWR_EN PMIC input coming from the…
Part Number: TPS65218D0 Other Parts Discussed in Thread: AM3351 , Tool/software: We are using the TPS65218D0 with the AM3351. We've measured 400us for the nPFO signal to be asserted from the time the PFI input drops below the 800mV threshold. See attached…