Part Number: TPS65219EVM-SKT Other Parts Discussed in Thread: TPS6521905 Hi,
Below is TPS65219EVM-SKT schematic but it's different from TPS6521905 pin map.
Pin number is shifted 90degree.
Which is correct?
TPS65219EVM-SKT
TPS6521905
Thanks. …
Part Number: TPS65219EVM-SKT Other Parts Discussed in Thread: USB2ANY , Hi,
At bring-up of EVM, there is connection error.
Error message is "Connected to USB2ANY Controller, but failed to connect to TPS65219x on I2C @0x30".
Procedure is as below…
Hi,
The output voltage of Buck1 can be re-programmed using one of the programming board at the following link: https://www.ti.com/tool/TPS65219EVM-SKT . The programming guide also explains the in-circuit programming steps using an external USB2ANY. Here…
Part Number: TPS6521905 Other Parts Discussed in Thread: TPS65219EVM-SKT , , TPS65219
Hi,
I have checked the operation of TPS6521905 using TPS65219EVM-SKT. However, I tried to change the output voltage of LDO3 from 1.2 V to another value, but it did not…
Hi Lillian,
Both the above mentioned EVMs will come with default programmed ICs. There is no burn process necessary to start evaluation.
For the TPS65220: Use the TPS65219EVM (same silicon). This IC is reprogrammable but the IC will come with default…
Hi,
Thanks for reaching out! What processor or SoC are you powering with the TPS65219 PMIC? TPS65219 02 is a pre-configured device that was programmed to meet the power requirements of the Sitara AM62/AM64 processors. This device has all the power rails…
Part Number: AM6422 Other Parts Discussed in Thread: TMDS64EVM , TPS65219EVM
Hello expert,
AM6422+TPS6521903+DDR4 is using on our project.
One unit is found that it can boot up and reset(by RESET_REQZ and MCU_RESETZ) normally, but system will be halted…
Hi,
Thanks for reaching out. For Artix-7 FPGA, I have listed three options below. Please let us know if there are any questions.
TPS65023B
This is a hardware configurable PMIC with reference design available.
Link to Reference Design: https://www.ti…
Hi,
In addition to the TPS6521901-04, we also have new variants that have not been released yet. If we get more information about the application use case like input supply and DDR memory, we might be able to identify a NVM config.
The socketed EVM…
Hi Kyoung,
The TPS65219 can support DDR3.
Here is a general block diagram showing the TPS65219 connection to AM335x:
If this connection scheme fits your needs, we can generate a CSV file for you. This file can be used to load the proper register settings…