Part Number: TPS65223-Q1 Other Parts Discussed in Thread: TPS65222-Q1 , Tool/software: Hi Team,
We require TPS65222-Q1 part datasheet. Please provide us as soon as possible.
Regards,
PNS
Part Number: TPS65223-Q1 Tool/software: Hi, TI
There is any information for I2C_1 Address? (TPS6522312-Q1)
I checked full datasheet for TPS65223-Q1, but cannot figure out that Address.
Part Number: TPS65223-Q1 Tool/software:
We use TPS65223Q1,and output voltage is OK,but the pin 27: INT/EN_DRV is low ,we have pull up at other side,could you guied why the pin 27 output low?
Thanks!
Part Number: TPS65223-Q1 Other Parts Discussed in Thread: LM5141 Tool/software: Hi Expert,
During high and low temperature tests, it cannot start at -40 degrees, but it can start when the temperature is adjusted to -30 degrees.
Please help confirm…
Part Number: TPS65223-Q1 Tool/software: Hi Team,
my customer is using TPS65223-Q1 to power TDA4, they test TPS6522312RAHRQ1 on their board, all outputs work well except BUCK3 is 0, is 0V the default output of BUCK3? If not, what is the check points…
Part Number: TPS65223-Q1 Other Parts Discussed in Thread: TPS65222-Q1 Tool/software: Hi Team,
As we are performing the Functional safety analysis, we require few details related to one your part number (TPS65222-Q1)
Failure modes
FIT rate
Failure…
Part Number: TPS65223-Q1 Tool/software: Hi Team,
I looked at the data sheet best I can but I did not see a PGOOD pin. nRSTOUT indicates power up sequence completed but I am not sure if it indicates power good state. I have seen that other TI PMICs have…
Part Number: TPS65223-Q1 Tool/software: i've got a design with the tps65223-q1 implementing the pdn-7a5 power config. this powers the pmic from 5.0v. on power up, i see the sw1 rail start to run for about 6.2ms, then it shuts down. this repeats some number…
Part Number: TPS65223-Q1 Other Parts Discussed in Thread: TPS65224 , , AM620 Tool/software: Hi PMIC experts,
Could you please confirm if the PMIC supports 5V operation.
Are there any differences with respect to TPS65224 that customer needs to be aware…
Part Number: TPS65223-Q1 Other Parts Discussed in Thread: TPS65224 Tool/software: Hi PMIC expert,
Can i use the GPIO4 and GPIO5 as ADC inputs.
Are both the inputs fail-safe
I see GPIO5 mentioned as fail-safe in the TPS65224 data sheet
Regards…