Part Number: TPS65233 Tool/software: Hi
I'd like to have the schematic reviewed, but I can't disclose the contents. Can you tell me how to send it personally?
And I have questions below.
1. Is it okay if the value of the inductor used for the LX…
Part Number: TPS65233 Background: We are having an issue with our products SW when controlling TPS65233 over I2C. Root cause is in the software that we currently cannot prevent it reading 0x2 register from the LNB controller. By unfortunate coincidence…
Part Number: TPS65233-1 Table 6.3 Recommended Operating Conditions specs the Junction Temperature range from -40 to 85 C, but calls it Ta. Does the table mean Ta (ambient temperature) or Tj (junction temperature?
Part Number: TPS65233 Other Parts Discussed in Thread: LM34936 Hi,
For LNB Power management TPS65233 can be used to get a voltage of either 13V or 18V. For meeting AISG Application requirement range between 10V to 30V are there any suitable devices from…
Part Number: TPS65233 Tool/software: WEBENCH® Design Tools Hi,
Can i get the power dissipation for this device for a 12V i/p Rail and 18V o/p rail at 0.4A load condition
Regards,
Sudarshan
Part Number: TPS65233
Hello,
I have mounted TPS65233 IC on breakout board and all the discrete components are placed on general PCB. Input given is 5.5V. Connections are made
I have checked short on all pins before connecting power supply and when I…
Part Number: TPS65235 Other Parts Discussed in Thread: TPS65233 , Tool/software: Hi
Previously, shorting the VCP and GND of TPS65233 caused the ic to burnt. At that time, TI guided the addition of diode to VCP as attached file. I'm going to use TPS65235…
Part Number: TPS65233 Greetings,
I want to select a suitable PMIC for my product, but I cant seem to find the exact match.
I have a single 3.7V battery, and an external 5V charging source,
and I need to operate from the battery and provide at least…
Part Number: TPS65233 Hi,
Earlier we used to Power the TPS65233 with 5V and generated the 13V/18V for the LNB. Also the same 5V was provided to the VCC pin(Pin #3) of TPS65233. We are now changing the Vin to 12V , in that scenario should we connect the…