Part Number: TPS65235-1 Other Parts Discussed in Thread: TPS65235 , TPS652353 Tool/software: We are using a TPS65235-1 with Rset of 330k. This means that our current limit should be at 440mA.
However, we are finding that the current limits at about 370…
Part Number: TPS65235-1 Other Parts Discussed in Thread: USB-TO-GPIO2 Tool/software: Wanting confirmation on if the TPS65235-1EVM-747 comes with a USB-TO-GPIO because UG says 'The EVM kit includes the USB-TO-GPIO interface box' But it also says…
Part Number: TPS65235 Tool/software: Hi
In order to do LNB Out Voltage control VSET[3:0] , should EN and VCTRL pin be open without connecting anything?
Thanks
Part Number: TPS65235 Other Parts Discussed in Thread: TPS65233 , Tool/software: Hi
Previously, shorting the VCP and GND of TPS65233 caused the ic to burnt. At that time, TI guided the addition of diode to VCP as attached file. I'm going to use TPS65235…
Hi Leif,
We have not seen an update from you for one month, so I assume the questions are answered and the issue is solved.
If you don't have any further questions, can you please close the thread by clicking on resolved. Clicking the Resolved Button…
Part Number: TPS65235 Hi,
Could you tell me the worst case power consumption in certain modes of the TPS65235 and how this could be calculated.
e.g. 12V input/ 18Volts output/ at 600mA load/ with diseqc. 140mΩ power MOSFET running at 1 MHz
Thanks…
Part Number: TPS65235 Hi,
I have been looking at designing an LNB which is controlled by DiSEqC signalling and found this IC. From reading the datasheet it appears that IC provides a +13V/+18V signal with the 22kHz. Is it also possible to use this IC…
Part Number: TPS65235-1
Hello,
Our customer has a question if TPS65235-1 has a potential issue in his application.
In his application, 12.7V boost input voltage is dropped to 12.4V for 10ms then back to 12.7V, while it works 19V VLNB. Even though he…
Part Number: TPS65235
Hi
May I know the main difference between TPS65235 and TPS65235-1? By comparing the both datasheets, it seems like the only difference is the support of FCCM.
I have two questions:
If we are not using FCCM mode, then TPS65235 could…