Part Number: TPS65235
Hi
May I know the main difference between TPS65235 and TPS65235-1? By comparing the both datasheets, it seems like the only difference is the support of FCCM.
I have two questions:
If we are not using FCCM mode, then TPS65235 could…
Part Number: TPS65235 In comparison table from the link below Max Iout of TPS65235 is 0.65A and TPS65235-1 is 1A.
However, both TPS65235 and TPS65235-1 datasheet shows Iout max is 1A.
We would like to know which one is correct for TPS65235?
if both TPS65235…
Part Number: TPS65235 Hello, we are facing a problem with the voltage amplitude of the DiSEqC signals. Is there a way to increase it above 750 mVpp? We would need this feature because a few costumers have some multi-switches that need a amplitude up to…
Part Number: TPS65235 Hi, TI expert.
A customer has an inquiry about the Fall time of SCL signal of I2C Interface of TPS65235.
If you look at the datasheet, the MIN spec is 20ns.
However, if you actually measure it, it is measured as 12.859ns. (see SCL…
Part Number: TPS65235 Hello, we currently have a case of using TPS65235, and the customer has reported a problem: When 22K is turned on, the cable detection mechanism of TPS65235 will cause false positives. The simple schematic diagram of our board is…
Part Number: TPS65235 Hi,
Our customer asking do we have TPS65235 alternative part, the same Vin/Vout/Iout condition, but do not need DiSEqC protocol support.
Thanks!
Jeff
Part Number: TPS65235 Hi,
I just wanted confirmation that I can use TPS65235, TPS65235-1, and TPS652353 interchangeably if I am not concerned about the audible noise?
Need a confirmation that these are functionally and PCB footprint wise same.
Due to…
Part Number: TPS65235 Hi
In non- I2C mode, what is happening when EN is floating?
When user's system in standby mode, the GPIO is not activated causes the EN pin floating.
Engineer observed the EN pin is in high state. Is it necessary to add a pull…
Part Number: TPS65235 Hi Team,
Our customer wants to check if we have power on reset function inside for TPS65235, can you help to check it? Also, if under some situations, the I2C bus for this device becomes abnormal, do we have any recommended procedure…
Part Number: TPS65235-1 Other Parts Discussed in Thread: TPS652353 , Hello,
Our customer asked about how TPS65235-1, TPS652353 respond if he accesses unassigned I2C register like 0x03. Do TPS65235-1, TPS652353 respond anything like ACK for example.
best…