Part Number: TPS65251 Hi,
Per our datasheet and EVM user guide, our recommend resistor for the CMP pin is 20k, 0.1% accuracy.
Could we use 1% accuracy resistor in stead of?
Thanks.
BR
Mason
Part Number: TPS65251 Hello guys,
One of my customers is considering using TPS65251 as a FPGA power supply of their new products.
They are looking for a calculator for peripheral parts selection like Webench or Excel base file?
Do you have any calculator…
Part Number: TPS65251 Hi Team,
Can I remove an inductor while all the output ENABLE pins are in enable mode and expect that hiccup mode will not be induced by removing an inductor?
I was unable to determine if hiccup mode is entered through an internal…
Part Number: TPS65251 Hi,
We are using TPS65251-1RHAR in our SMT. But the pins looks like black and can not pass SMT machine(somethinglike a Optical Inspection System to assist SMT location ) to next step. Can anyone help me to check what can we do?
Part Number: TPS65251 We have designed a board using this component. Two copies of the board have shown the same behavior and we have been unable to understand what has happened (so as to modify future designs incorporating this part). Schematic is attached…
Part Number: TPS65251 Hii,
Please provide us the Sample Calculation (with some example) to find the values of Compensation Parameters (Rc, Cc, and Ccomp) for the "9.2.2.1 Loop Compensation Circuit" in DataSheet.
Part Number: TPS65251 Hi,
My input voltage is 12V, O/p of buck1 = 3.3V, Buck2 = 2.5V, Buck3 = 1.8V.
1. During the bringup, the EN of Buck1 is toggling i have checked the input ripple which is around 500mV.
2. When i am checking the datasheet there where…
Part Number: TPS65251 Hi Team,
Could you show the difference between TPS65251 and TPS65251-x, as well as difference between TPS65251-1, TPS65251-2 and TPS65251-3?
I looked at the datasheet but didn't find...
thanks a lot.
Best regards,
Yang