Part Number: TPS652510 Hi: I'm using the TPS652510 to generate three outputs, input is 13v-9v, outputs are 1.5V, 5.4V and 1.8V. Most of the current is on 1.5V around 2A, 5.4V and 1.8V loads are light which are around 100mA. There are some weird ripple…
Part Number: TPS652510 Hello:
I'd like to know if you have some simulation tool of TPS652510. I'm using it on a new design right now. The input is between 9-13V, and output is 1V, 5V and 8V. Since it's a mobile product, the input is a battery voltage…
Part Number: TPS652510 Last time when i made used all three outputs ( 5V,9.6V and 3.3V respectively) from 12V input I was facing a voltage drop at 9.6V when I load the 9.6V. So this time I disconnected the output side of channel 2 as shown. But now both…
Part Number: TPS652510 Hi: I'm using the TPS652510 to generate three outputs, input is 13v-9v, outputs are 1.5V, 5.4V and 1.8V. Most of the current is on 1.5V around 2A, 5.4V and 1.8V loads are light which are around 100mA. There are some weird ripple…
Part Number: TPS652510 Good Day!!
As Part of one of Our projects, We are using " TPS652510RHAR" Buck converter for the conversion of 3 voltages 5V, 3.3V and 9.6V from 12V.
Our Requirement is
Input Voltage: 12V
Output 1: 5V,3A
Output 2: 9.6V…
Part Number: TPS652510 Other Parts Discussed in Thread: TPS65261 , TPS65261-1 Hi Experts,
Our customer is going to use a Spartan 7 FPGA from Xilinx as the control device. For its power supply (1V, 1V8, and 3V3), He is considering the use of a PMIC…
Part Number: TPS652510
In the internal diagram of the IC we can see that there is a 1uA current source for the Enable pin,
1) how id this 1uA generated?
2) Will this charge the capacitor and increase its voltage to above the enable voltage and enable…
Part Number: TPS652510
When I power the circuit, the voltage output drops from 9.6V to 8.4V for a load of 270mA.
The 5V and 3.3V are not loading even at higher current.
Hi Gerold:
I understand, but the issue is that this part is not supported in WEBENCH. I was wondering if there was a similar single rail part that I could choose in WEBENCH to design each of the TPS652510 rails. I want to this part on a new design because…
Part Number: TPS652510 Hello!
We plan to replace TPS65251-x with TPS652510 because of components shortage.
Question is: what happens if we conenct Vin=12V supply to the NC pins 32, 33, 34 of TPS652510RHAR to avoid any PCB modification? Is it acceptable…