Part Number: TPS65252 Hi I am using TPS65252 in one of my designs and one of the cards I was debugging and found that Enable 1 & 2 are continuously pulsing and hence the outputs are not coming. Can you please let me know what may be the reason.
V7V…
Part Number: TPS65252 Hi,
Any one please suggest me, If USB section is not used in my application, then USB pins can be connect to GND or VCC or left as Not connected.
And what happens when connected USB section pins(23,25,26,27 and 28 pins) to GND?
…
Part Number: TPS65252 Hi,
Assuming that the USB_VO pin is not active, disabled by 0v on the USB_EN pin. Is it safe for a user to connect a USB 5v source of power to the USB_VO pin. I am trying to avoid putting a diode or a switch inline with the USB_VO…
Part Number: TPS65252 Hi,
we want to design in our TP65252.
We don't get support from distributors, so I contact you directly.
Is it possible to get a contact person?
We have some questions to this power ic.
Thank you
Kind regards
Johannes
Part Number: TPS65252
When the USB current limit is triggered, it seems that the TPS65252 part heats up immediately and goes into thermal shutdown eventually.
I tried this with many different values for rUSB, limiting down to 200mA. During normal operation…
Part Number: TPS65252 Other Parts Discussed in Thread: TPS54383 Hello,
I am looking at using the TPS65252 configured with 9v input and 5v and 3.3v outputs. I see that the EVM for the TPS54383 (similar part) is supplied in this configuration (5v and 3…
Part Number: TPS65252 Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models Hello Team,
TPS65252 TINA Average Reference Design transient analysis shows VOUT1 becomes 94.24V at 1.1ms.
Could you help to provide a correct TINA…