Other Parts Discussed in Thread: TPS65252 , TPS65283 Hi team,
We are working with the TPS65252 and we have a few questions:
Currently we are seeing 0.4V at pin LX2 when connecting pin EN2 to ground. What could be the reason for seeing this?
Should we…
Other Parts Discussed in Thread: TPS65252 Hi.
Implementing 3 buck using 2 TPS65252, buck1 is 3.3V, buck2 is 1.2V, buck3 is 1.8V.
And max requirement delay time is 1.5ms, 2ms between each sources as 3.3->1.2->1.8 sequence.
So, I set EN capacitor…
Hi, Jordan
I review your schematic, it is okay, but layout is bad.
I think the issue is caused by bad layout, suggest place 30ea VIAs at thermal pad.
I attached a layout guideline for your reference.
TPS6525x_LAYOUT_GUIDE.ppt
Part Number: TPS61252 Other Parts Discussed in Thread: TPS65252 , Hi,
I'm reviewing TI's TPS65252 for my application, but this device works at active-high.
Is there any active-low device simular spec with TPS61252?
thanks,
TS
Other Parts Discussed in Thread: TPS65262 , TPS65252 Hi! Can i powering Sitara processor with TPS65262 like a TPS650250 ? Important to use processor in NITRO mode. I understand that the DVFS / SmartReflex™gear won't work. It means that voltage VDD_MPU…
Other Parts Discussed in Thread: TPS652510 , TPS65253 , TPS65252 Hi Team!
I am planning to use a TPS652510. However, I was not sure about the PGOOD pin when one of the bucks is disabled. I would imagine that the PGOOD output would only depend on the state…