Part Number: TPS65261-1 Hi,
We got a question from customer about TPS65261-1
Could you help us?
[Question]
Can the output voltage be set from the feedback voltage 0.6 V ?
Is it possible to output less than 1.0 V ?
Thank you
Best regards
Part Number: TPS65261-1 Other Parts Discussed in Thread: TPS65261
Tool/software: WEBENCH® Design Tools
Hi team.
I did simulation for TPS65261-1 via WEBENCH.
However, the bode plot result of Vout3 was output in a different form than normal.
It is…
Part Number: TPS65261-1 Hello Non-Isolated DC/DC Experts,
Do we have temperature cycling data for the TPS65261-1? Mechanical stress due to temperature cycling?
Part Number: TPS65261-1 Dear TI Team,
Would you help this request?
Integrate the PWM signal of the SoC as shown in the figure below and connect the signal to the DC-DC FB Check if DC-DC output voltage control function is available. -.ex) R1 : 13.3 kΩ, R2…
Part Number: TPS65261-1 Hi,
We got a question from the customer about TPS65261-1. Could you help us?
[Question] They are considering using the EN pull-down resistor. How much is the recommended range of EN pull-down resistor?
Best Regards, tateo
Part Number: TPS65261-1 Hi team.
My customer has inquired about multiple Input/Output capacitors connected in parallel.
Please tell us what problems you may encounter if you use several capacitors with low capacitance instead of one capacitor with high…
Part Number: TPS65261-1 Hi team.
My customer designed the power with the TPS65261-1.
He designed 12V input circuit and 5V input circuit.
He want to verify the circuit .
And he want to recommend capacitor capacity in compensation circuit.
I hope to share…
Part Number: TPS65261-1 Hi team.
My customer designed the power with the TPS65261-1.
He designed 12V input circuit and 5V input circuit.
He want to verify the circuit .
And he want to recommend capacitor capacity in compensation circuit.
I hope to share…
Part Number: TPS65261 Other Parts Discussed in Thread: , TPS65262 , TPS65263 , TPS65265 , TPS65268-Q1
Hi support team.
In the May 2023 datasheet, the recommended capacitor for V7V of the following models have been changed from 1-μF to 10-μF.
TPS6…