Part Number: TPS65262 Hello Team,
in case I do not use an LDO of the TPS65262 , what would be the recommended state?
Can I just disable it via LENx and leave the output floating?
Or would you recommend to have a minimum load as well to keep the pass transistor…
Part Number: TPS65262-1 Hi,
What will be the impact on performance(or on IC) if I power the IC with Single-cell Li-Ion battery(@ 3V min.) when there is no AC/USB supply ??
Thanks in advance.
Part Number: TPS65262-2 Hello, customer will use TPS65262-2 powering the Altera FPGA. it requires voltage accuracy from ext. DC/DC power shall be within +/-2.7% for 1.1V rail.
How to calculate the output voltage accuracy of the TPS65262-2 with 1% tolerance…
Part Number: TPS65262 Other Parts Discussed in Thread: TPS65263-Q1 , In the datasheet, it doesn't not specify the ambient temp in the recommended operating conditions. what's the amb temp?
Also, in the abs max. ratings which says the Tj is up to…
Part Number: TPS65262-1 I'm not using BUCK3 and I require the Pgood signal. If I want to use the automatic sequencing (MODE = HIGH), how should I connect the following pins:
VIN3
BST3
LX3
FB3
EN3
If I choose not to use the automatic sequencing (MODE…
Part Number: TPS65262-1 I seem to be up against a brick wall. I have a design using a TPS65262-1
Input 12 V
Out1 5V
Out 2 3.3V
Out 3 2.5 V
Lin 1 1.8 V
Lin 2 2.2 V
The 5 Volt is enabled immediately (if input is above a set minimum). The others come…
Part Number: TPS65262-1 I am using the TPS65262-1 to deliver the following voltages
Buck 1 = 12V input, 5V output
Buck 2 = 5V input, 3V3 output (5V is supplied by output of buck 1)
Buck 3 = 5V input, 1V2 output (5V is supplied by output of buck 1)
…
For designed TNR-3770CF project for ADB, we use TI TPS65262-2RHBR DC/DC converter. In default it is set to NOT use pulse skipping mode.
Our customer requested to reduce power consumption in deep standby. Due to technical reason (design validated) we would…