Part Number: TPS65262-1
Dear Team ,
We have planned to use the TPS65262-1RHBT IC in one of our project . 1 Our requirement is 1st BUCK2 output have to get 2nd is and
BUCK 3 have to get the output
then after BUCK1 have to enable
2 LEN1 and LEN2…
Part Number: TPS65262-1 Hi,
I have a TPS65262-1 regulator configured to output 3.3V on BUCK3. LVIN1 and LVIN2 are connected to the output of BUCK3 (3.3V). LDO1 is configured to output 1.2V, and LDO2 is configured to output 1.66V. I would like to enable…
Part Number: TPS65262-1 Other Parts Discussed in Thread: TPS65262-2 , Hi Experts,
Our customer is using TPS65262-2 on their board but due to the stock issues, they will be using TPS65262-1 for replacement on a design they already fabricated.
The customer…
Part Number: TPS65262-1 Other Parts Discussed in Thread: TPS65262-2 , Hi Team,
What's the difference between TPS65262-1 and TPS65262-2?
Thanks and Best Regards!
Hao
Part Number: TPS65262-1 Hi,
I am designing using TPS65262-1, but my prototype having some issues with the design. I had designed two LDO to output 1.2V and 5V with input voltage 3.3V and 5.5V respectively.
But the actual voltages in the prototype is 0…
Part Number: TPS65262-1 Other Parts Discussed in Thread: TPS65262-2 Hi team,
Customer found TPS65262-1 will enter PSM mode at light load. Do we have P2P device that has forced PWM mode? Thanks
Part Number: TPS65262-2 Other Parts Discussed in Thread: TPS65400 Tool/software: Hi Team,
I am using the PMIC part TPS65262-2RHBT in my design. I need to sequence the outputs of this PMIC. LDO1 output should enable Buck 1 and Buck1 output should enable…
Part Number: TPS65262-1 Hi,
What will be the impact on performance(or on IC) if I power the IC with Single-cell Li-Ion battery(@ 3V min.) when there is no AC/USB supply ??
Thanks in advance.
Part Number: TPS65262-1 I'm not using BUCK3 and I require the Pgood signal. If I want to use the automatic sequencing (MODE = HIGH), how should I connect the following pins:
VIN3
BST3
LX3
FB3
EN3
If I choose not to use the automatic sequencing (MODE…