Part Number: TPS65262-1 Other Parts Discussed in Thread: TPS65262-2 , Hi Team,
What's the difference between TPS65262-1 and TPS65262-2?
Thanks and Best Regards!
Hao
Part Number: TPS65262-2 Other Parts Discussed in Thread: TPS65262 Dear TI members,
I need a ref TINA file for checking phase margin / gain margin of TPS65262-2
I can't fine it on TI website.
Best regards
Part Number: TPS65262-2 Hi TI Team,
We are planning to use TPS65262-2 for generating on-board supplies for different interfaces on our board from 5V input. The requirement and our plan is as below
Buck 1 for 3.3V, 3A supply
Buck 2 for 2.5V, 1A supply …
Part Number: TPS65262-2 Hello Our customer is applying TPS65262-2RHBR. The applicable specifications are as follows. VIN = 5 V Voutput = Buck 1 / 3.3V, Buck 2 / 3.3V, Buck 3 / 1.5V problem
1. Buck2 is Enable, but PWM output is 0V.
2. Buck3 is Enable, but 2…
Part Number: TPS65262-2 Hello, customer will use TPS65262-2 powering the Altera FPGA. it requires voltage accuracy from ext. DC/DC power shall be within +/-2.7% for 1.1V rail.
How to calculate the output voltage accuracy of the TPS65262-2 with 1% tolerance…
For designed TNR-3770CF project for ADB, we use TI TPS65262-2RHBR DC/DC converter. In default it is set to NOT use pulse skipping mode.
Our customer requested to reduce power consumption in deep standby. Due to technical reason (design validated) we would…
Hi Cameron,
It's not recommended to connect the inputs of two LDOs and the outputs of two LDOs to get parallel LDO, because the equaled current flowing in 2 LDOs can't be assured. Thus they cannot be used in parallel. If the 2 LDOs are used in parallel…
Part Number: TPS65262-1
Dear Team ,
We have planned to use the TPS65262-1RHBT IC in one of our project . 1 Our requirement is 1st BUCK2 output have to get 2nd is and
BUCK 3 have to get the output
then after BUCK1 have to enable
2 LEN1 and LEN2…
Hi Kygo,
I have listed the closest matches below: - TPS650330 https://www.ti.com/product/TPS650330-Q1
- TPS65262 https://www.ti.com/product/TPS65262-2
- TPS65811 https://www.ti.com/product/TPS65811
Thank you.
Regards, Alex