Part Number: TPS65263 Please advise if possible to bake the Aptiv Part Number 28445108 - IC-VR,BUCK,TRIPLE faster Email: mateusz.nowara@aptiv.com Company: APTIV Company phone: Language: English State: Open Provide case details or comments:
APN Dimension …
Part Number: TPS65263-1Q1 Hello,
Do you have any theoretical material for Loop Compensation (but section 8.2.2.4 of the datasheet )?
Is it necessary for output voltages? If not, what should be dome with those 3 pins?
Thanks!
Part Number: TPS65263-1Q1 Other Parts Discussed in Thread: TPS65263
Hey Team,
a customer is having an issue with sine wave current ripple of 290 mV and 30 kHz due to periodic changes of power consumption at a sensor.
Output is at 480 mA and 1.26 V.
…
Part Number: TPS65262 Other Parts Discussed in Thread: TPS65263 Hello team,
I am not using LDO1and LDO2. What should I do for the unused pin below?
LVIN1, LVIN2
LOUT1, LOUT2
LFB1, LFB2
LEN1, LEN2
Also the capacitor value recommended for V7V pin is 10uF…
Part Number: TPS65263-Q1 Tool/software: WEBENCH® Design Tools sir, design has been referred from webbench and model with .tsm format has been used from TI even then output is not appropriate .
Part Number: TPS65263-Q1 Other Parts Discussed in Thread: TPS65263-1Q1 , Hi team,
Could you please help to share the difference between TPS65263-Q1 and TPS65263-1Q1?
Thanks!
Part Number: TPS65263-1Q1 I have a 67 % DC square wave, 1 Mhz, wich i want this TPSxx to syncronize to. This is exactly the switch node voltage of another buck, cascaded on the out of CH1 of TPS65263-1Q1.
Datasheet explains that:
-the active sync edge…
Part Number: TPS65263-1Q1 HI.
in my application, i have ch 2 & 3 ENx floating (=immediate start at power on). Ch1 has a 1 uF cap to ground on it's EN1 pin, delaying it's start about 200mSec
How do i have to expect PGOOD to behave then?
In…
Part Number: TPS65263-Q1 Other Parts Discussed in Thread: TPS65261 , TPS65263 , TPS65400 Tool/software: WEBENCH® Design Tools Hi,
have inherited a design with this chip. It come with values, for compensation networks, that semt well working.
In order to…