Hi Jason,
Jason Reinhart said: Only the TPS65263 Pspice Average Model folder has a complete project that I'm able to load and run.
The other folders, including the TPS65263 TINA average model folder you seem to be recommending do not have complete…
Part Number: TPS65263-1Q1 Output voltage range for TPS65263-1Q1 Buck1, 2 and 3 with the use of external resistors at FB Pin is not been mentioned in datasheet.
Could you please provide the info.
Thank you!
Part Number: TPS65263-1Q1 Hello TI experts,
My customer drew their first schematic with TPS65263-1Q1. Could you review the schematic?
and here are some questions.
1. They don't want to use I2C communication for setting.
Is it okay to set ENx…
Part Number: TPS65263-1Q1 Hello,
Do you have any theoretical material for Loop Compensation (but section 8.2.2.4 of the datasheet )?
Is it necessary for output voltages? If not, what should be dome with those 3 pins?
Thanks!
Part Number: TPS65263-1Q1 Other Parts Discussed in Thread: TPS65263
Hey Team,
a customer is having an issue with sine wave current ripple of 290 mV and 30 kHz due to periodic changes of power consumption at a sensor.
Output is at 480 mA and 1.26…
Part Number: TPS65263-Q1 Other Parts Discussed in Thread: TPS65263-1Q1 , Hi team,
Could you please help to share the difference between TPS65263-Q1 and TPS65263-1Q1?
Thanks!
Part Number: TPS65263-1Q1 I have a 67 % DC square wave, 1 Mhz, wich i want this TPSxx to syncronize to. This is exactly the switch node voltage of another buck, cascaded on the out of CH1 of TPS65263-1Q1.
Datasheet explains that:
-the active sync…
Part Number: TPS65263-1Q1 HI.
in my application, i have ch 2 & 3 ENx floating (=immediate start at power on). Ch1 has a 1 uF cap to ground on it's EN1 pin, delaying it's start about 200mSec
How do i have to expect PGOOD to behave then?
In my application…
Part Number: TPS65263-1Q1 Hello,
My customer has question of switching frequency of TPS65263-1Q1.
In data sheets, it is written about SW frequency min 430kHz typ 500kHz max 560kHz.
Can they think it's accuracy -14%~+12%, when the setting of…