Part Number: TPS65266 Tool/software: Hello ,
We have used TPS65266RHBT multi-switcher IC to meet specific parameters for our project. Here are the requirements: Input Voltage: 5V Output1: 0.9V @ 3A Output2: 1.5V @ 1.5A Output3: 1.8V @ 1.5A
for which after…
Part Number: TPS65266 I noticed in the data sheet for the TPS65266 that the minimum operating temperature is ‑30 °C, which seems a little unusual. Is this really the case, or might it be a typo … we need operation down to ‑40 °C.
Hi Jay,
I would suggest you can check loop stability with below Pspice average model.
TPS65266 Unencrypted PSpice Average Model Package (Rev. A)
Thanks!
BRs
Lucia
Part Number: TPS65266 Hi I have a question regarding the function of the enable pins of the TPS65266: I have a design where I control the enable pins with an MCU. I noticed that one of the regulators still outputs a voltage (lower than the voltage set…
Part Number: TPS65266 Hi team,
Could you provide the tolerance of EN discharge time at the start up(typ 2ms) in the format of xxms~xxms or +/-xx%?
Guarantee is not required. It's just for reference information.
Best Regards,
Part Number: TPS65266 Other Parts Discussed in Thread: LP8758 Hi,
I had used TPS65266RHBR in my previous design of board. But there is slight change in the design and I am looking for a new PMIC with below requirements:
Vin(typical)= 3.3V
Vout 1: 1.1V Iout1…
Part Number: TPS65266
Hi,
I am using TPS65266 in my design. I have attached the schematics. Can someone please review the schematics and let us know your feedbacks on the same.
My requirement is as below.
1488.PMIC.pdf 1. Vin=5V
2. Buck1: Vout=1.8V Iout…