Part Number: TPS65266EVM-686 Other Parts Discussed in Thread: TPS65266-1 Hi Team, how can we evaluate the TPS65266-1 on this board? Is there a setting needed to be done?
Thank you.
-Mark
Part Number: TPS65266-1 Hi,
We are using TPS65266-1 in our design to generate 1.5v, 1v & 1.8v.
Attaching the schematics. Please review and let us know if the discrete values at each output are correct.
L8, L9, & L10 value-2.2uH
Thanks,
Tejasw…
Part Number: TPS65266-1 Hi, TPS65266-1 support team
I am thinking to suggest TPS65266-1 to customer as the power solution for the power supply of PCI Express SDD. But I have a concern if TPS65266-1 can support the power on sequence of PCI Express M.2…
Part Number: TPS65266-1 Hi, TPS65266-1 support team
What power sequence will become when Css is common and the only PWR=3 has a delay time as Figure 1?
I think it's either Figure 2 or Figure 3, but which is it?
What is the correct power sequence…
Part Number: TPS65266-1 Other Parts Discussed in Thread: SWITCHERPRO , , TPS65266 Tool/software: WEBENCH® Design Tools Is there a loop compensation design tool for TPS65266-1? Do you have another tool other than Webench, like to old SwitcherPro standalone…
Hi Alex,
It's not a typo. T he minimum operating temperature of TPS65266-1 is ‑30 °C, while TPS65266's is -40℃. If operation down to -40℃, recommend to use TPS65266.
Best regards,
Zhou
Part Number: TPS65266 Hi,
If someone can tell me what is the difference between TPS65266 and TPS65266-1?
I saw the Vout(min) of TPS65266-1 is 2.7V on the web but on datasheet TPS65266-1 can output 1.2V.
I was confused...
Part Number: TPS65266 Tool/software: Hello ,
We have used TPS65266RHBT multi-switcher IC to meet specific parameters for our project. Here are the requirements: Input Voltage: 5V Output1: 0.9V @ 3A Output2: 1.5V @ 1.5A Output3: 1.8V @ 1.5A
for which after…
Part Number: TPS65266-1
Hello,
Please clarify my doubts related to TPS65266-1 regulator below:
1. How to control(Enable/Disable) Outputs of the DC-DC regulator: TPS65266-1 ??
2. Is there any possibility of getting a Switched voltage regulator with…
Hi Stanley,
Thanks for coming to us with your queries.
We have TPS65266-1 which is p2p with TPS65266. The main difference between TPS65266 and TPS65266-1 is the behavior in light load condition. One is PSM and the other is FCCM.
BTW, what is Vin, Vout…