Part Number: TPS65279 Hello,
I am considering this part for a 6V to 5V conversion at 1.6MHz. This results in an ON time of 521ns, and an OFF time of 104ns.
How can I verify the voltage droop of the bootstrap capacitor during this ON time?
Will…
Part Number: TPS65279 Other Parts Discussed in Thread: TPS54290 , TPS65261 hi,
we are designing in w/ TPS65279 and need to set a current limit lower than 5Amp (in the range of 2-2.5).
we need to know more details about accuracy of current limiter…
Part Number: TPS65279 Hi
My customer has some queries need help.
The issue is when using TPS65279VRHH power management IC on our development board.
We are using 12V as VIN, and expect is 1.8V for VOUT2 and 1.2V for VOUT1, which we currently using…
Part Number: TPS65279 Hi
My customer has some query need help.
The issue is when using TPS65279VRHH power management IC on our development board.
We are using 12V as VIN, and expect is 1.8V for VOUT2 and 1.2V for VOUT1, which we currently using…
Other Parts Discussed in Thread: TPS65279 Hi team,
Did we have the TPS65279 can do the siulation?
If not, when will we have the TPS65279 on the WEBENCH for simulation?
Thanks,
Scott
Part Number: TPS65265 Other Parts Discussed in Thread: TPS65279 , Hello Experts,
Is it possible to club together the 3 outputs of this chip to get 10A output?
In what all combinations can the three outputs be clubbed together to get more current…
Part Number: TPS65400-Q1 Other Parts Discussed in Thread: TPS65279 , LM61460 , LM62460-Q1 , TPS7H4010-SEP Hello,
I've been shopping for a while trying to identify the best buck regulators for a design that will have:
14V < Vin < 18V
Vout1 = 12V…
Hi, Peter
1. For the peak current control mode, the output voltage can be close to Vin.
However, when Vout is big, duty is big, high side MOSFET will turn on more time, because of high side MOSFET's Rdson is big, IC will have thermal problem, the…
Josh,
This device uses D-CAP mode instead of Peak Current Mode, so do not support phase interleaved. Yes, will submit request to correct the parametrics for this device.
If you are seeking phase interleaved devices, please refer TPS65279.