Part Number: TPS65295 Hi. I have a question about the value of resistor R1 at Figure. 31 in the datasheet.
Can I omit this resistor?
What is the maximum allowed value for R1?
Best regards.
Part Number: TPS65295 Hi Team,
Do you have pin FMEA document of TPS65295?
In particular, I would like to know the following results.
1. adjacent pins short
2. Each pin open
Regards.
Miyano
Part Number: TPS65295 During light load conditions, the part operates at discontinuous conduction mode as stated in the datasheet. In this mode, when SW and SW_VPP output become high impedance, output voltage temporarily exceeds the absolute maximum rating…
Part Number: TPS65295 As per datasheet TPS65295, Vddq(1.2V) is giving 8A, Vpp is giving 1A and Vtt is giving 1A of current. So, the current values are for single dimm.
Can I use this for DDR4 with 3 DIMM ?
Can you suggest any power supply for 3 DDR4 DIMM…
Part Number: TPS65295
As per the datasheet and reference design, the BST pin has a 5.1 ohm resistor. The reference design used an 0603. What's the current going into the BST pin, or the power on the BST resistor? Would be nice to know for derating…
Part Number: TPS65295 Hello Team,
The minimum PVIN voltage is 4.5V in recommended operating condition. How this value is derived?
Please let me know the least limitation of PVIN. Is it concerned with IVDDQOUT?
What is the possible phenomenon when PVIN…
Part Number: TPS65295 Hi,
I see the power decoupling guidelines that make use of 10uF, 1uF, 0.1uF caps on a single voltage rail. Does this create issues with resonance? Since I have 1uF caps in the same 0402 size as 0.1uF caps, I would like to simply use…
Part Number: TPS65295 Hi,
I'm using the TPS65295 in my design which doesn't need to support the S3 state. In this case, can the SLP_S4 and VTT_CNTL inputs be shorted and controlled be a single driving source to enable/disable the device? Also, the datasheet…