Part Number: TPS65296 Hi team,
The customer has doubts about the power consumption calculation of TPS546D24RVFR and TPS65296RJER.
In this formula Power Loss = ( Vout * Iout )*( 1/η − 1), η It is only an estimate, but not an accurate value.…
Part Number: TPS65296 Hi expert,
Our customer use our TPS65296.
They find that we just show typ output voltage in DS.
They want to know the min and max value of the output voltage.
Could you help on it?
Thanks
Best Regards
Sean Song
Part Number: TPS65296 Good afternoon,
I have an issue with switching node of VDD1 and VDD2 when the load is light.
'TPS65296: Vmin of switch exceeded during light load', I already see this created issue but I couldn't see the solution proposal.…
Part Number: TPS65296 Hi Sir,
After power on, the shell temperature of TPS65296 rises above to 85 ℃ quickly (Ambient temperature 25 ℃ ). Then the power chip triggers the thermal protection mechanism.
What are the possible reasons for this phenomenon…
Part Number: TPS65296
Hello,
We noticed that the package drawing information of TPS65296 doesn't match the real component footprint.
Is Texas Instruments aware of this issue or I just receive a counterfeit part?
Best regards,
Marco
Part Number: TPS65296 Dear sir,
Please help to check if the schematics design is ok or not, thanks!
PVIN = 12V
PVIN_VDD1 = 5V
Load: Micron LPDDR4 4GByte * 2pcs
This PMIC is design for the power supply of LPDDR4 , so we don't need the LDO channel, my doubt…
Part Number: TPS65296 Hi all,
There is TPS65296 as a power supply to LPDDR4. Is there any product other than TPS65296 that supplies power to LPDDR4? I hope to configure multiple power products and input to LPDDR4. Please tell me the recommended product in…
Part Number: TPS65296 Hi Team,
Tps65296 supplies power to lpddr4x, but there is abnormal pulse on vdd1/vdd2/vddq output voltage.Take vdd1 output as an example.