Part Number: TPS65310A-Q1 Tool/software: HI BU team
Is there the device ID information in tps65310A-Q1 registers to make customer to know the device is tps64310A-Q1?
Thanks
Part Number: TPS65310A-Q1 Hello,
The app note for this IC shows how to calculate buck elements for 2 amps approximatively.
What about a design with 200mA? Does the compensation network equations are still correct?
Best
Part Number: TPS65310A-Q1 Hello,
I would like to know, what is the pin FMEA for pins 9, 11 and 13 for the TPS65310 ATIC in the open condition.
Thanks
Edgar
Part Number: TPS65310A-Q1 Hello,
Vbuck 3 (1.2V) seems to be instable: when reaching 1.2V after 1ms there is a big ripple (200ms) and after1.2ms the chip stop to work( P fet activated). I suspect it's the UVLO and OVLO on the buck 3 due to the high…
Part Number: TPS65310A-Q1 Hi Team,
We have a customer requesting for a SPI-based communication driver for TPS65310AQRVJRQ1. Do we have this type driver?
Regards,
Danilo
Part Number: TPS65310A-Q1 Can I run VIO at 2.5V? Will this cause the SPI to be 2.5V compatible?
V_VIOMON_TH looks like it trips at 3.13V, but there is note under the V_RESL electrical conditions that has VIO at 1.2V, so I figured I would double check…