Part Number: TPS65400 Tool/software: Hello,
My customer is testing the TPS65400 operation on a board they designed as shown in the circuit below.
TI_PMIC_TPS65400RGZT.pdf .
When they measured VDDA, VDDG, and VDDD after inputting VIN 12V and CE high…
Part Number: TPS65400 Tool/software: Hello,
I am triyng to use TPS65400 for generating 4 indipendent voltages, each one with different regulation; in general Ioutmax = 0.3A and Vout = 7...9V. The control of the Ic is made with I2C protocol.
The schematic…
Part Number: TPS65400 Tool/software: Hi,
I designed a custom project using the TPS65400 and based the schematic on the EVM.
At startup, only LP_3V3 is enabled, powering low-power 3.3V circuits, which draw around 100mA-200mA.
Here are my measurements…
Part Number: TPS65400 Deam Team,
We are used TPS65400 power management IC as a buck converter as like below voltages
input voltage: 24V
out 1 : 5Volts
out 2 : 8Volts
out 3 : 3.3Volts
out 4 : 3.3Volts
we designed circuit as per suggested…
Part Number: TPS65400 Tool/software: Hi Team,
PMBUS command can sets the VREF
Burn the program into EEPROM before assembling the IC
Please provide TPS65400 Programming example code (.hex)
Thanks
Part Number: TPS65400 Hello
My customer is considering using the TPS65400 in two types: current sharing and non-current sharing as shown below.
Please review the customer designs below to see if there are any problems.
TPS65400RGZ current share…
Part Number: TPS65400 Ti Support Team,
I want to simulate Bode plot for my Custom Design.
I am using Pspice for TI.
Also Downaloaded Transient and Average Pspice models of TPS65400.
In one of the TI post come to know that need to use Average model…
Part Number: TPS65400 Hi team
Please have a look on question below from the designer:
"just a question regarding the ripple limits and this, just to clarify something we saw during the analysis…
Look this image:
These are the values between…
Part Number: TPS65400 Hi Team,
Customer is testing TPS65400 in their design, but found the default PWM switching is DCM mode in light load, but the datasheet description is CCM in default, can you help to double check whar's the default mode for this…
Part Number: TPS65400 Tool/software: We are using TPS65400 to generate 3.3V in Channel 1 and 1.1V in Channel 2, and 1.35V in Channel 3, 2.5V in channel 4.
We got output during Board bring up stage, later when we Tuning the Compensation Network to…