Part Number: TPS65400EVM-678 Other Parts Discussed in Thread: USB2ANY
Tool/software:
Hi, I read the forum post here about putting firmware 1.19 onto the USB2ANY in order to fix issues.
TPS65400: USB2ANY: Problems connecting usb2any to tps65400 …
Part Number: TPS65400 Hello,
My customer has requested accurate efficiency information for the usage conditions below.
Please provide usage efficiency values for the five cases below.
CASE 1
Device
Input Voltage
Input Current
Output…
Part Number: TPS65400 At present, we use TPS65400QRGZTQ1 chip, the input is 5V, and the output voltage is 4, respectively 1.8V@2.5A max 1.1V@2.5A max 3.3V@2.5A max 3.3V@400mA max I am currently designing the schematic for T-Box products used in automobiles…
Part Number: TPS65400 Other Parts Discussed in Thread: TPS65263 Tool/software: Hello,
My customer is looking for step-down (buck) products between 3A and 15A with output voltage/current monitor function via I2C or PMBUS.
The products I found are 8…
Part Number: TPS65400-Q1 Tool/software: Hello,
We have an automotive application and were looking at the TPS65400-Q1 since it meets all of our specs.
However, we need to understand what the noise spectrum looks like when the device is configured for…
Part Number: TPS65400 Dear team,
Our customer has to adjust the PMIC compensation loop. They see ripple in the 1V line and would like to mitigate it adjusting the compensation loop as well.
They checked an application note SLVA352A regarding the compensation…
Part Number: TPS65400 Hi,
Are there any Linux driver for TPS65400 PMBUS? My customer wants to TPS65400 PMBUS Linux driver.
If there are PMBUS Linux driver for any devices, please advise us.
Thanks and best regards, M.HATTORI.
Part Number: TPS65400 Hi,
Is it possible to use TPS65400 as a standalone? I would like to run TPS65400 without using I2C or SMBus.
Best Regards,
Nishie