Other Parts Discussed in Thread: TPS65631W Hi All,
We hae three quesitons for TPS65631W,
1.tscp in datasheet page 11 value is the spec page 5(tscp=10mS)
2. The input voltage range can support 4.8V or not , since the battery votlage is higher and higher…
Other Parts Discussed in Thread: TPS65631W , TPS22860 , SN74LVC1G132 , SN74AHC1G00 Hi
I have a customer making smart watch. They have chosen two AMOLED supplier, one is RM69080, the other is RM67160. The two AMOLED Displays need differnt Power Supply. For…
Other Parts Discussed in Thread: TPS65631W Dear. TI
I'd like to calculate the max SW current on TPS65631W following the document "Application note, SLVA372C"
The load current would be just max 50mA.
I think that the I LIM(min) value should…
Other Parts Discussed in Thread: TPS65631 , TPS65631W The TPS65631 and TPS65631W are popular devices for powering OLED displays in wearable applications. The displays used in these applications are quite small and consume much less current than the maximum…
Part Number: TPS65632 Other Parts Discussed in Thread: TPS65631W Hi team,
Customer is using RT4731, we are promoting our solution, is TPS65632 a suitable part for this application? Could you suggest a proper part for this application?
Thanks and Best…
Part Number: BQ25150 Other Parts Discussed in Thread: BQSTUDIO , TPS65631W , BQ25155 , EV2400 Hello:
Currently, when debugging BQ25150, I encountered two problems as follows:
1.Most of the time, the PMID foot will output the voltage value close to the VBUS…
Other Parts Discussed in Thread: TPS65631W , TPS65633 HI All,
If the input voltage of TPS65631W is higher than 4.5V/4.6V, can we still get 4.6V output ? Do we have a official document for this question. I noticed that we have one similar application…