Part Number: TPS65680 Hi Team,
Could you advise me on an alternative part for LT4380? P2P solution? OCP/ OVP/ Surge Protect/ Reverse Voltage Protect
Vin 5.5 - 65V, 20A
Thanks
Part Number: TPS65680 Hi
May i ask few questions as below:
1. Can i just use CLK1 ~ CLK 8 as below configuration and left rest of the CLK pin not used ?
2. How to configure the data of C1~C6 and D1~D3
3. Can i change the value of t5 and t6 in the excel…
Part Number: TPS65680 Hi,
Will TPS65680 have AEC-Q100 grade version in the future?
If yes, what is the schedule?
If no, will we have alternative part for automotive customer?
Thanks a lot.
Best regards, Cage.
Part Number: TPS65680 Hi all,
Need your help for the VGL1, VGL2 voltage application question as following:
Does any issue or concern once the VGL1/VGL2 work in -2V or close to -0V as example due to the recommneded operating conditions for VGL1/VGL2 are…
Part Number: TPS65680 hi,
my customer is planning to build a prototype board to test TPS65680 performance. customer plans to provide a timing table to TI at first, then needs TI BU hlep generate a config file. Therefore,could you help share a time table…
Part Number: TPS65680 Hi, All
Customer program the OTP memory four times are OK, but can't program once more.
Is the a possible of OTP memory size not enough??
If yes, may I know how much size of OTP memory?
Part Number: TPS65680 Hi, All
As the attachment picture. When we set 0xFF bit[1] = 1, what is the different with 0xFF bit[1] = 0?
As the description of 0xFF bit[1], this has a different when we execute reload.
What is the reload, load data from OTP…