Other Parts Discussed in Thread: TPS65721 , TPS65720 HI
I have a question about Voltage Setting
In TPS65721, both DCDC1 and LDO1 are externally adjustable.
but datasheet page.36 description
For reference only: A voltage change in the register will not have…
Other Parts Discussed in Thread: TPS65720 , TPS65721 I was looking at the application circuit for the TPS65720 and TPS65721 - on the BGA version, the 65720, there is an input capacitor of 2.2uF on VINLDO1.
On the circuit for the 65721, there is no input…
On a side note, this device suspends charging at 45C range. You can move the range up or down depending on your liking but, increasing the range is difficult even though possible by changing the NTC and resistor network on the battery pack. In general…
Other Parts Discussed in Thread: TRF7970A , TPS65720 Hi All,
One of my customer is looking for Schematic Symbol and footprint library of below devices. This information is not available in website.
TRF7970A
TPS65720
Please provide me ASAP, we are running…
Other Parts Discussed in Thread: TPS65720 , TPS65721
On page 43 of the TPS65720 / TPS65721 datasheet, it says: "A feed-forward capacitor in parallel to the resistor from Vout to FB_LDO1 is required. It´s value should be based on transient performance…
Other Parts Discussed in Thread: BQ27210 , BQ27410-G1 , TPS65720 Hi,
I have a question about the bq27410-G1 and bq27210 gas gauges. I try to decide which gas gauge to use. I have a 130mAh LiPo built in battery in my application. The pack only integrates a…
Other Parts Discussed in Thread: TPS65010 , TPS65720 , TPS65070 Hello,
I've an question about the Charge Status register (CHGSTATUS 0x01) on the TPS65010. I'm configuring the charger by default (CHGCONFIG = 0x1B) so the fast charge timer and taper timer…
hi
i am having a doubt regarding the smps in pmic
the output current in it is higher than input current and voltage(vice versa) buck converter.....how do we get higher current at the o/p (transformer analogy) as the smps switches on/off with the feedback…
Other Parts Discussed in Thread: TPS65721 DEARS.
1. If PB_IN is applied during the operation? 2. Does PB_IN Timing starts again from the beginning?
3. How To Reset the TPS65721? Because the need to control the output of the DC/DC output and LDO output…