Part Number: TPS659037 Other Parts Discussed in Thread: AM5728 , Hi,
I am using TPS6590379ZWST to power up AM5728 and other peripherals in my board. I need to change voltage and sequence for my application. Kindly clarify the below
In TPS6590379ZWST TRM…
Part Number: TPS659037 Hi team,
It is nice to know you here. My customer needs TI to provide a qualification report for them, I cannot find it on TI.com. Please help provide it to them. Thanks.
BR,
Charles Lin
Part Number: TPS659037 Other Parts Discussed in Thread: AM5746 Hi. there.
I use TPS6590379 for power up to AM5746.
And I refer the design idkAM574x board.
I meet the issue.
SMPS9 is not working.(0V)
but other LDOx and SMPSx output correct voltage.
…
Part Number: TPS659037 Other Parts Discussed in Thread: AM5716 , TMDXIDK5718 Hi
I am making a board similar to the MDXIDK5718 and checking the operation, but AM5716 and TPS6590379 reset alternately as shown in the attached figure, and AM5716 does not start…
Part Number: TPS659037 Our customer designs a board using AM574x with TPS6590379.
Some of the VRTC digital input pins are pulled-up to the VRTC power rail to be fixed high. But the output current of LDOVRTC while the PMIC is in OFF state should not exceed…
Part Number: TPS659037 About schematic and layout for TPS6590378, I have question about SMPS1_2_FDBK_GND and SMPS4_5_FDBK_GND pin setting.
Application note: TPS659037 Design Guide is described below;
But TPS659037 Design Check List is described below…
Part Number: TPS659037 Other Parts Discussed in Thread: TMDSEVM572X , , TMP102 , AM5728 In our custom board based on the TMDSEVM572X evaluation board, an error that the power could not be turned off, happend to our customer enviroment. In the debugging of…
Part Number: TPS659037 Hi,
Using the external oscillator, 2.2uF is required.
If this 2.2uF is nothing(OSC16MCAP pin is opened), can the external oscillator work?
I recognize to degrade the accuracy of the frequency in this case at least.
Best Regards…