Part Number: TPS659037 Other Parts Discussed in Thread: AM5726 Hi Expert,
My customer design the custom AM5726 board
What is the defference TPS6590376ZWSR between TPS6590378ZWSR?
Is pin to pin?
TPS6590376ZWSR is not available now.
Could I replace TPS6…
Part Number: TPS659037 Other Parts Discussed in Thread: AM5728 Hi, we have one board following AM5728 GP EVM design, in which there is an external DCDC buck regulator generate 5V from ACDC power. This 5V is the input of TPS6590378 LDOUSB and LDO12. Our…
Part Number: TPS659037 Ref to TI doc. User's Guide TPS659037 SLIU011F and Datasheet SLIS165G:
There are 2 versions of application TPS6590378 and TPS6590379 with either 3V3 or 5V Main supply in the Users Guide
the datasheet says: All the LDO inputs can…
Part Number: TPS659037 Other Parts Discussed in Thread: TPS65916 sliu011f User's guide is described "The TPS659037 device should be used for AM571x when PCB compatibility between an AM572x and AM571x board is required." on page 2.
Please…
Part Number: TPS659037 Hi,
My customer requests Internal power supply information.
Which power supply(VCC1 or VRTC or another) does supply for following each block/pin?
Peripheral circuit of OSC16MIN, Peripheral circuit of OSC16MOUT, Internal CR oscillator…
Other Parts Discussed in Thread: TPS659037 I need to learn how a PMIC such as TPS659037 works. How do you set the output voltage? How does it change the output voltage (does it do it automatically? and if so, how does it do it? Can output voltages be adjusted…
Part Number: TPS659037 Hello support team.
I'm considering the peak current of inductor.
However, I can't find the current maximum limitation of SMPS in datasheet.
Should I think of it as IOmax?
Best regards.
Higa
Part Number: TPS659037 Hi, From the application note (SWCA302A), I understand that there are three conditions for POR generation. • The VCC1 supply has a falling slew rate less than 90 mV/ms between 1.9 V and 1.8 V. • The VCC1 supply has a rising slew…
Part Number: TPS659037 When I studied product datasheet for TPS659037(SLIS165C, SLIS165E and SLIS165G), as far as I came to know, older TPS6590376 and new TPS6590378 are pin compatible. Same thing is with TPS6590377 and TPS6590379. The Power Up sequencing…
Part Number: TPS659037 Other Parts Discussed in Thread: AM5728 , , TMDSEVM572X , TPS53319 Hi,
TPS659037 is used with AM5728 in our design, based on TMDSEVM572x. There is no separate power on switch on the board. What is the connection required on BOOT0 &…