Part Number: TPS65910A3EVM-583 Other Parts Discussed in Thread: AM3352 Hi Expert,
Customers currently use AM3352
AM3352 does not control TPS65910A3 to run at 600Mhz with preset voltage
Customers want to use I2C2 to control the TPS65910A3 to run…
Part Number: TPS65910A3EVM-583 Other Parts Discussed in Thread: TPS65910 , TPS65910EVM After start-up and when load is dropped we observe the 3.3V VMMC to go up to 3.6V or even higher. Afterwards we see the voltage dropping normally slightly below 3.3V…
Part Number: TPS65910A3EVM-583 Other Parts Discussed in Thread: TPS65910 I am using am335x-GP-evm and trying to enable and use RTC available on PMIC. I am refering below thread and did changes to dts for tps & kernel config CONFIG_RTC_TPS65910=y.
…
Part Number: TPS65910A3EVM-583 Other Parts Discussed in Thread: TPS65910 , USB2ANY , IPG-UI Customer is using TPS65910A3EVM-583 EVM for evaluation.
They observed no output at:- VDIG1, VDIG2 & VAUX33. J10 & J8 are installed on the EVM. Any additional…
Part Number: TPS65910A3EVM-583 Other Parts Discussed in Thread: TPS65910 Hello,
Regarding to ILMAX register on TPS65910AA1, my customer is asking some question.
They use 600MHz(@OPP100) on AM3554, currently ILMAX register of VDD_MPU is configured…
Part Number: TPS65910A3EVM-583 Other Parts Discussed in Thread: TPS65910 In AM335X EVM Board without booting the processor we are getting PMIC Output VDIG1=1.8V, VMMC=2.45V . The same PMIC is used in my customized board where i am getting VDIG1=2.4V,…
Part Number: TPS65910A3EVM-583 Other Parts Discussed in Thread: TPS65910 Tool/software: Linux HI,
we are using pmic TPS65910A31A1RSLR in Am335X , supplier don't have the same IC's, so that they are suggesting alternate part TPS65910A3A1RSLR
can we…
Part Number: TPS65910A3EVM-583 HI ,
We are using TPS65910A3 as the PMIC for our AM335X based Board .
The PMIC is having a pin "nRESPWRON " . I am having a bit of a confusion with the pin . It is suggested to connect this pin to the "PWRONRSTn" of…
Part Number: TPS65910A3EVM-583 Other Parts Discussed in Thread: AM3352 , TPS65910 Hello,
Have a customer use TPS65910A3 PMIC for AM3352, have some questions about PMIC TPS65910A3.
1. The output voltage and sequential of TPS65910A3 follow below tables…
Part Number: TPS65910A3EVM-583 Hi ,
I am using TPS65910A3 to design my power system.
I have one key(or two keys ) use as a power on (power off) key.
Should I connect the button to which pin of TPS65910A3?
Thank you so much.