Part Number: TPS65911 Hello,
We purchased the parts of PS659118A2ZRC from Rochester, and under the X-RAY, the sizes of solder balls are different. While the appearance is not noticeable
Pls check the below picture for details.
Could you help to…
Part Number: TPS65911 Hello,
We want to use 32.768KHz crystal outside of TPS65911 to calculate system time.
Our product use under -5C---50C temperature range, we can correct crystal and system time under 25C, could you tell me how to make crystal…
Part Number: TPS65911 Other Parts Discussed in Thread: TPS65910 Hi All,
Currently I'm facing a problem that I add some code to set the TPS65911 INT_MSK_REG(0x51) register to value 0xfb in the kernel driver as the code wroted below.
static int…
Part Number: TPS65911
Hi support team,
TPS65911AA2NMAT outputs other than VRTC are not output.
The situation is similar to the "Original question" above. Has the EEPROM program problem improved? Please let me know the measures.
Regards, Dice-…
Part Number: TPS65911 Hi support team,
Is it prohibited to make OSC32KIN floating when neither "BYPASS CLOCK" nor "CRYSTAL OSCILLATOR" is used? Should I connect OSC32KIN to GND?
Regards, Dice-K
Part Number: TPS65911 Hi team,
We can see from the ti.com that TPS659112A2ZRCR is suspend production.
Customer want to use TPS659112A2NMAR as replacement.
Could you please help check if they need to change the hardware and software?
And if there…
Part Number: TPS65911
Hi support team, Continuing from the "Original question" above.
Is the VDDCtrl current limit by RTRIP Resistor detected by the Low Side Valley current?
In that case, I think that "(IOUTmax - inductor-ripple-current/2)" is…
Part Number: TPS65911
Hi support team, About SWCS049S.
I think that IOUTmax should be added to the equation (6).
And I think that equation (2) becomes equation (6) with the above correction.
Is my interpretation correct?
Regards, Dice…