Part Number: TPS65911 Other Parts Discussed in Thread: TPS65910 , Hi All,
Our device using the TPS659114A2NMAR as the PMIC, and our kernel version is 4.1.15.
In our expectation, we thought that when we press the power button, the INT1 need be set…
Part Number: TPS65911 Hi support team, Continuing from the "Original question" above.
Why does "TPS65911A Typical Application" recommend 12V or less?
Is it to ensure ON DUTY of about 10%? Is it to avoid lower conversion efficiency?
Regards, Dice…
Part Number: TPS65911 Hi support team,
In the figure below, there is a description that the external FET power supply is 12V or less.
Is it possible to use 3~25V according to the electrical characteristics?
For example, I want to use 18V.
…
Part Number: TPS65911
Hi support team,
Is there any specification for the pull-up destination of SDA_SDI and SCL_SCK? The datasheet is pulled up to VDDIO. Is it possible to pull up by 3.3V that input to VCC6?
Regards, Dice-K
Part Number: TPS65911 Other Parts Discussed in Thread: CSD87330Q3D , 66AK2G12
Hi support team, This is a confirmation about VDDctrl parts selection. I would like to confirm how to calculate the inductor and Rtrip.
What design requirements led to…
Part Number: TPS65911 Dear Specialists,
By related thread, the boot issue was fixed from shipped out on August 19, 2021.
Normally, the date code(Red Box) is the production date, and the SEAL DATEIESAL DT) on the left side of the label is the shipping…
Part Number: TPS65911 Hello there,
I am testing PN TPS659113A2ZRCR for counterfeit and found the following as the die markings : TPS65911A2, PG1.2
Was hoping to get an answer if the following die markings are consistent with PN TPS659113A2ZRCR.
…
Part Number: TPS65911 Other Parts Discussed in Thread: 66AK2G12 The current scheme is: SOC(66AK2G12) + PMIC (TPS65911A).
The problem is: VCC5V0_DCDC normal, VRTC is 1.8V. However, ViO does not output 3.3V normally, resulting in VDD1, VDD2 without normal…
Part Number: TPS65911 Other Parts Discussed in Thread: 66AK2G12 Dear Specialists,
My customer is considering TPS65911AA2NMAT and has a concern.
Customers are concerned that the TPS65911AA2NMAT may not boot from EEPROM.
I would be grateful if you…