Part Number: TPS6593-Q1
I noticed that the Datasheet documentation mentions:
Hardware Integrity up to ASIL-B / SIL-2
Systematic Capability up to ASIL-D / SIL-3
Could you please help us understand how this should be interpreted from an ISO…
Part Number: TPS6593-Q1
Hi Team,
I am currently evaluating the TPS6593-Q1 as the power management solution for one of our ASIC designs.
The ASIC core rail operates at 0.75V with a peak current requirement of approximately 3.38A , and the target…
Part Number: TPS6593-Q1 Other Parts Discussed in Thread: TPS6521905 Hi,
Thank you for the recommendation of TPS6593-Q1 instead of TPS6521905. We are ordering the EVB for it. Do you have any PMICs with primarily LDOs and maskable RV checks?
Do you…
Part Number: TPS6593-Q1 Other Parts Discussed in Thread: TPS6594-Q1 Hi,
I open this thread for one of our customers. I will share the link so that he can answer potential follow-up questions.
In the datasheet and other related documents, there is…
Part Number: TPS6593-Q1 Hello,
I am currently programming a TPS6593-Q1 PMIC using a Scanflex 2 Cube Boundary Scan Controller via the MPP channels. Communication is done over I²C using the default PMIC address 0x28, and CRC is disabled.
We have observed…
Part Number: TPS6593-Q1 Other Parts Discussed in Thread: SCALABLE-PMIC-GUI Hi
I have a few questions regarding the use of TPS6593-Q1 in the early development stage.
If we purchase generic samples of TPS6593-Q1 and mount them on our own PCB, is…
Part Number: TPS6593-Q1 Following table shows two values for the 3 parameters. Which ones are the default factory settings? In our application, we don't want to change the default values. Thanks.
Part Number: TPS6593-Q1 Other Parts Discussed in Thread: AM62A3 , We normally need to test several parameters in order to evaluate the performance of a DCDC (or LDO) including ripple, phase margin, transient response, efficiency and etc..
But in this…
Part Number: TPS6593-Q1 In our TI AM62Ax , we are making use of the PTPS65931211RWERQ1 PMIC part for power management. We need to make use of the nPWRON/ENABLE pin as a power ON/OFF button with requirement as given below:
When the board is powered…