Part Number: TPS6594-Q1 Hello Experts, I am working on TPS6594-Q1 in Q&A mode, I have the following questions while reading the TRM:
What are the steps involved in reading the questions and writing the answers?
While/ after getting the answer from…
Part Number: TPS6594-Q1 Hello Sir,
Does TPS6594-Q1 support 5V input for VCCA while considering worst case?
The maximum threshold with 5V is 5.8V. And the minimum accuracy setting is 4%.
So the WCAS maximum threshold will be 6.032V which excluding 6V. …
Part Number: TPS6594-Q1 Hi Ti team,
For TPS6594, how to calculate the output inductor? Is it the same as DCDC?There is no formula in the datasheet.
Another question, if we need calculate the inductor for PMIC? Because I see that there will be a recommended…
Part Number: TPS6594-Q1 Hi, I am using PMIC having below details
Default value of Register WD_LONGWIN_CFG Register (Offset = 0x405) is 0xFF. Query:
As per default value 0xFF, Watchdog should timeout after 772 Sec and trigger a reset. But Its resetting after…
Part Number: TPS6594-Q1 Other Parts Discussed in Thread: LP8764-Q1 Dear expert,
Customer write tps6594-Q1 and LP8764-Q1 register and then read back to check.
How much delay they need to wait before check? Is there any special register they need to wait…
Hello Michele,
So the team has released a file, please do let me know if this works for you.
Attached here is the file: .tzr TPS6594-Q1 AEDT ICEPAK
BR,
Nicholas
Part Number: TPS6594-Q1 Hi, Expert.
As title description.
Customer try to use MCU control TPS6594x,
How to know TPS6594x work in which state?
For example, How to know TPS6594 works in "STANDBY Mode" ? I think ,
1. Could we read register from…
Part Number: TPS6594-Q1 Hi Team,
What do the two lines below the silk screen of TPS6594 material mean?
Can you help explain it to the customer in detail?
Part Number: TPS6594-Q1 Other Parts Discussed in Thread: MSP-EXP432E401Y 1、PMICA is TPS65941213;PMICB is TPS65941111
2、Scalable-PMICs-GUI version is 3.0.0
3、PB2 (SCL) and PB3 (SDA) linked to I2C1 of PMIC A using MSP-EXP432E401Y; PB2 (SCL) and PB3 (SDA) are…
Part Number: TPS6594-Q1 Hello I have written a configuration file for the nvm with the gui and tested it on the evm . but for some reason when programming the nvm on a pcb the nvm gets locked after 1 time ( I’m using the same file to burn both) .…