Hello Nicholas,
Nicholas McNamara said: Harsha, so to understand that you initially provided this post on the EVM, but you have a tps65941212 on a development board and you're trying to program it to power the Xilinx SoC.
Yes, Nicholas I had initially…
Part Number: TPS659413EVM Hi, first NVM programming with attached file was possible. After trying to program the PMIC with the same file, following messages were reported.
"EEPROM Unlock Failed" and "Please verify the program".
What…
Part Number: TPS659413EVM Hi Teams.
Our teams have a project which uses AM6528+TPS65941319RWER. Now I have two issues need to be solved.
1、5 Bucks and 4 LDOs are disable when power up because of default setting (Please see the attached picture), Should…
Part Number: TPS659413EVM Hello Team,
Our automotive customer is looking for 9-rails PMIC which sequences can be programmed freely.
They needs
Number of rails : More than 9
Voltage : 1.1V, 1.8V, 3.3V
Current : about 300mA ~ 500mA
I think TPS659413EVM…
Part Number: TPS659413EVM Hi,
In the EVM design, the series resistors R20 and R21 are used at the VSYS_SENSE pin. Both of them are 240ohm. My customer has a question that if those two resistors can be replaced by one 480ohm resistor? Is there any special…
Part Number: TPS659413EVM Dear TI.
Now I'm using TPS659413F0RWERQ1 & TPS659411F0RWERQ1 for TDA4VM chipset.
My understanding from PMIC datasheet, diagnostic function of voltage and current monitoring data is internally combined and output through…
Part Number: TPS659413EVM made a board with reference to the TDA4X EVM board, but the PMIC TPS6594113 and TPS6594111 are not working smoothly.
1. The first time the power is turned on, it works well 2. If the power is turned off and then turned on immediately…
Hi Harsha,
Please ensure that VCCA 3.3V is provided to the EVM.
Although it looks like you may have established I2C communication in this thread:
https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1190540/tps6594evm…