Part Number: TPS65982 Other Parts Discussed in Thread: TPS65981 , TPS65987 We have a product consisting of 2 parts, both are powered by battery. When one of the batteries runs out of power, the other can supply power to it through USB-TYPE C, it will source…
Part Number: TPS65982 Other Parts Discussed in Thread: TPS65981 , TPS65988DJ , Hi,
Good Day.
I have a question about software TPS65981_2_6_7_8 Application Customization 6.1.4, does it fit TPS65982DJ? I have a broken laptop and the SPI flash of this TPS65982DJ…
Hi Kevin,
Kevin Kosta said: These values are set up based on the PD contract and cannot be manually selected.
If the request current of PD contract is 3A, which setting will the TPS65982 select? Setting 14 or setting 15?
Thank you,
Leon
Part Number: TPS65982-EVM Other Parts Discussed in Thread: TPS65982 , , TPS65987 I have a USB 2.0 device connected to the mux on the TPS65982-EVM through the header pins and have been unsuccessful getting the USB 2.0 bus to enumerate. I have been trying…
Part Number: TUSB1046EVM Other Parts Discussed in Thread: TPS65982 , TPS65987 Hi there,
as some others have asked before, I also need the project files to customize some settings of the PD-Controller on the TUSB1046EVM.
Thanks in advance!
Jessica
Awesome, thanks for the good news and I am glad that I am able to provide my help. Please feel free to post additional questions to the e2e forum if you need technical help.
Thanks
David
Part Number: TPS65982 Other Parts Discussed in Thread: TUSB546EVM Hi,
In the TUSB546EVM, GPIO2 from TPS65982 is connect to the POL signal line. May I know how to enable the PD controller to output the logic according to the orientation of the cable plugged…
Part Number: TPS65982 Other Parts Discussed in Thread: TPS65987 Hi Team,
TPS65982 has an external spi flash where it can boot and load appcode.
Can you kindly help me to understand whether the following is correct:
1. TPS65982 detect the Vbus, boot and…
Part Number: TPS65982 Other Parts Discussed in Thread: TPS25750 Hi Experts, Good day. so it will take me some time to understand everything in the datasheet, so the quick question is: will this chip behave in the following ways: 1. Being capable of using…