I removed R41, R43, & R44. When I now attempt I2C communication, I get an acknowledgement from a device at address 0x12.
Thank you very much for your assistance.
Part Number: TPS65986 hello guys
I'm Trying to make some USB-C dock with "TIDA-01243" Reference Design
and i'm trying to make some modification.. like remove of external barral jack..
anyway, I found TPS65986 was obolsete, and found…
I was able to program the TPS65981EVM following your instructions and it worked. I tried programming a second TPS65987EVM and for some reason it is not behaving the same. When I power it up and connect it, it constantly resets as if it can't negotiate…
Part Number: USB-CTM-MINIDK-EVM Hi,
Does the TPS65986 comes with any FW or I need to program it ?
At USB-CTM-MINIDK-EVM - which program burned in the TPS65986 by default ?
Thanks
Asaf
Part Number: TPS65986 Hi all,
We have compatible issue about PD connection in TPS65986 PDO 20V3A to some NB. We test different version FW (from 1.11.02 to 1.38.06), modify peak current setting to 200% but can't solve the issue.
But when we test…
Part Number: TPS65986 Hi all,
I see in datasheet the ILIMPP5V in table with listing of 16 possible settings of it. Also I see the in datasheet: "Settings selected automatically by application code for the current limit needed in the application.". But…
Part Number: TPS65986 Hi, I'm looking for a chip or set of chips that can help me support both a USB-C data connection for a camera and display port video at the same time. The camera would be an output and the displays an input. I need two displays…
Hi David,
Please let me know if this is correct, I can just use USB C to USB 3.0 cable or adapter?
TUSB564RNQEVM = TUSB564 and TPS65986 won't need firmware = jumpers setting is it true?
What should I do with CC pins on USB C in this case?
Thank you…