Part Number: TPS65986 I am reading the TPS65986 Reference Manual and register 0x32 TX Source Capabilities Register Bit Field Definitions has 7 32-bit fields for PDO Contents. How is the 32-bit field for PDO contents defined? Also, is there an example…
Part Number: TPS65986 Hi Sir ,
I need help on customizing firmware for TPS65986 device using Application Customization Tool version 4.01.
Here i required option to change below configurations on Application Customization Tool version and generate a bin…
Eric,
I tried a similar scenario on my EVM and it seems to be working fine. Could you provide some CC and PD logs so I can take a closer look into it. Also, when you were testing after you detached it, did you check the VBUS directly on the device? If…
Part Number: TPS65986 Hello, I believe the TPS65986 supports/complies with USB-PD revision 2.0, is that correct? Is there any plan to support USB-PD rev3.0 with this device, or is that support limited to the '987D device? Thank you.
Part Number: TPS65986 Dear Sir,
we now have a design for TPS65986+HD3SS460 full function TYPE-C(host), and got a problem as below:
1. we don't know how to config the GPIO2 for POL signal in Application Customization tool(3_11), can you help to send…
Part Number: TPS65986 Would like to understand all cases where TPS65986 will effectively re-boot from SPI-Flash. Understand that POR event will do this, but have also been told that all PD HardReset events will cause this as well. However, experimentation…
Part Number: TPS65986 Hello Team
i have designed a new PCB bard with the TPS65986, the PCB board is sort of a display board.
the board need to be connected to a Mini PC computer and need to power the mini PC.
can you support on how to configure the TPS65986…
Part Number: TPS65986 Hello,
This question relates to our TPS6598x devices, particular in a system similar to our mini-dock reference design: TIDA-01243
The section of the design I am curious about is the power path from USB-C UFP (port where the board…
Part Number: TPS65986
1. Can PD sink descriptor be updated dynamically from I2C command? I am looking for updating iManufacturer field.
2. The PD source should be able to read iManufacturer of connected sink device using I2C.
The above method will…