Part Number: TPS65988 Tool/software: Hi,
We are planning to use the TPS65988 in one of our ongoing projects. While going through the datasheet, I noticed that the TPS65988 supports an internal bidirectional switch for VBUS.
However, the reference designs…
Part Number: TPS65988 Tool/software: Hello Team,
We are currently developing a device on which we use TPS65988.
Our configuration will be as the following:
port A as sink and source (sink at 20V@3A, source 5V only), dual role data
port B as source…
Part Number: TPS65988 Tool/software: Hi,
We have an application where main system power is provided by one of the two ports managed by the TPS65988. So since the embedded controller (EC) won't be up by the time the TPS65988 negotiates power, the configuration…
Part Number: TPS65988 Tool/software: Can you please send me the PPC_Host TIVA firmware to allow debugging our prototypes that use the TPS65988. We will not be using this in production. It will be used solely to debug our hardware.
Hi David,
1.5uH would be okay for 800kHz and your schematic has the correct IADPT pin resistance. Yes, you should add the VSYS current.
Best Regards,
Jibin
Part Number: TPS65988 Other Parts Discussed in Thread: , TUSB1064 Tool/software: Hello:
I'm designing a new type docking station which require two TYPE-C with DP input, and I choose TUS1064 for crosspoint switch, I'm going to choose TPS65988 for the…
Part Number: TPS65988 Tool/software: Can I have the source files of TPS65988EVM? I have purchased the board and I would like to get the files or at least a better schematic PDF. Kind Regards,
Part Number: TPS65988 Tool/software: Hello,
I would like to use TPS65988 for my project. However, it seems that there are several different versions of TPS65988 e.g. TPS65988DH, TPS65988DJ and TPS65988DK. May I know what is the difference between these 3 parts…
Hi Eric,
v6.1.4 is the current version of TPS6598x GUI.
Eric Koch said: Can you flash my binary ( tps_bug.zip ) I attached two week ago and do a raw register feed as well?
Using the tps_bug.pjt these are the raw register read results using debug mode in…
Part Number: TPS65988 Other Parts Discussed in Thread: TPS65987 , TPS25751 Hello TI -
Our client is wondering what can be done from within the constructs of the TPS65988 - it's internal registers or it's interrupt events (which may or may not be enabled…