Hi Clarence,
TEST.PD.PROT.SRC.08
TEST.PD.VDM.SNK.01
TEST.PD.VDM.SNK.07
These are tester issues that I have confirmation for so we can close all issues on port B.
For port A we need to make a modification to the VIF to set swap to DFP supported to no f…
Part Number: TUSB1064 Other Parts Discussed in Thread: HD3SS214 , , TPS65988DK Tool/software: Hi
we have a new project call RSW, it is used for USB & DisplayPort switch for two host, we select TUSB1064 + hd3ss214 for its part function implementation…
Part Number: TPS65988DK Other Parts Discussed in Thread: TUSB1064 , , HD3SS214 , TPS65988 , TPS65987DDK , TUSB564 Tool/software: Hi
we have a new project call RSW, it is used for USB & DisplayPort switch for two host, we select TUSB1064 + TPS65988DK + hd3ss214…
Part Number: TPS65988DK Other Parts Discussed in Thread: TPS65988 Tool/software: Hello TI Team,
Can we connect two SPI flash over single SPI interface in USB PD TPS65988? \
This is simply to give option for 2x configuration file loading in USB PD via…
Part Number: TPS65988DK Other Parts Discussed in Thread: TPS65982 , TPS6598X-CONFIG Tool/software: Hello,
We are unable to programm the flash memory using the FT2232HL Programmer & TPS6598X-CONFIG — TPS65982 Configuration Tool. Below are the…
Hi David,
Apologies for the delayed response, seems like you were able to root cause the issue! If you need further assistance please open a new e2e thread for further support.
Thanks and Regards, Raymond Lin
Hi David,
Perfect, sorry for the delays in communication.
That was actually the issue I was running into, but didn't realize you had both external paths populated. During testing with the EVK, I was able to get the solution working if both sink paths…
Part Number: TPS65988DK Other Parts Discussed in Thread: TPS55288 , BQ25628 , BQ25798 Dear Team,
customer application as below in blue
Will this product only provide power input and output? No data (USB…), right? Master is Device A/B. This product…
Part Number: TPS65988DK Hi,
Would you please share TPS65988DK UL2367 cert #: 20190107-E169910 and IEC62368-1 cert #: US-34617-UL, certification and report to our local FAE contact window?
Ko, Zoe <zoe_ko@ti.com>
Thanks!
Jeff