Part Number: TPS65988DKEVM Other Parts Discussed in Thread: TPS65988 , Tool/software: Hi,
Schematics of the TPS65988 EVK with the FTDI circuit is readily available, however I have not found schematics for the TPS65988DKEVM which uses the TIVA debug circuit…
Part Number: TPS65988DKEVM Other Parts Discussed in Thread: TPS65988DK Hi,
I have TPS65988DKEVM. Could you please help me configure this device for the following scenario? I'll use these settings on my custom TSP65988 board as well.
Scenarios
1. USB…
Part Number: TPS65988DKEVM Other Parts Discussed in Thread: TPS65988DK Hello there,
Can I receive the config file(EEPROM data) on the FTDI debug board of the TPS65988EVM?
Thanks,
Sam
Part Number: TPS65988DKEVM Other Parts Discussed in Thread: TPS65988DJEVM Hi,
I'm working with TPS65988D in USB-C PD design. I got the schematic PDF and it's a little hard to understand about PCB layout. So, I would like to request for PCB project…
Part Number: TPS65988DKEVM Other Parts Discussed in Thread: TPS65988DK I will be using the TPS65988DK for a device that does not have a battery and only gets its power from USB. I can see SPI on the flash loads when powered by SYS_PWR, but when connected…
Hello David,
david hilderman said: Can you confirm that we can receive interrupts on I2C1_IRQ# and I2C2_IRQ# when cables are plugged/unplugged and when there are PD changes on the ports so that we can do the evaluation and set source capabilities?
Yes, you…
Part Number: TPS65988DKEVM Other Parts Discussed in Thread: TPS65988 , LM3489 , TPS65988DJ , TPS65988DJEVM , TPS65988DK We will be making a product that has 2 USB-C ports.
The product will run on 24 VDC but we will generate that from whatever voltage provided…
Part Number: TPS65988DKEVM Other Parts Discussed in Thread: TPS65988DK I am debugging TPS65988DK EVM.
When I connect the EVM with laptop and monitor as the picture shows using portB.
1. But the HPD_LED will not turn on and the video signal transmission…
Part Number: TPS65988DKEVM Other Parts Discussed in Thread: TPS65988DK
Hi Team,
I am attempting source 5V, 9V, 15V, 20V at 3A through ports A and B. Port B works for all the aforementioned values when a device is connected. However, when connecting a…