Part Number: TPS6598X-CONFIG Other Parts Discussed in Thread: USB-C-PD-DUO-EVM , TPS65981 , TPS65982 Hello Team,
when trying to set "Voltage Threshold as Sink Contract" on the USB-C-PD-DUO-EVM this error message appears:
Exception Encountered during…
HI, David.
1. I moved the R13 0 ohem resistor to R11.
2. You said "Can you also pull JMP10 high as well?" Maybe there is a typo. I made JMP9 (HPDIN)=3.3V ;
3. Connected CTL0 to GND, CTL1 to 3p3_VCC.
1&2, DP ALT not work;
1&3, DP…
Part Number: TPS65987D Other Parts Discussed in Thread: TPS6598X-CONFIG
Dear,
I have used the TPS6598X-config program well since I installed it last year to my WindowsXP desktop.
Last month I upgraded the OS to Windows7 (32bit), and everything works well…
Hi,
The USB-C-PD-DUO-EVM should be set to support 3A on each of the supported PDOs out of the box (5V, 9V, 15V, & 20V).
If you'd like to change the configuration on the EVM, you will need to download the TPS6598x-CONFIG GUI tool: https://www.ti…
Part Number: TPS65988EVM Hi,
I'm trying to control TPS55289 from TPS65988 via I2C. I followed the instructions in "Using I2C Master in TPS65987D and TPS65988 PD Controllers" ( www.ti.com/.../slvae18.pdf
Current setup:
TPS65988EVM: default…
Tomas,
Looks like TPS65988 could achieve the functionality you're looking for. I would suggest testing your configuration with the TPS65988EVM to confirm. The TPS65988 is a very flexible device and can be configured with the GUI tool. Here are some helpful…
Hello,
Damon Kelly10 said: Is it possible to get the tps65987D to also send charge current level commands to the battery charger when not connected to USB (i.e. powered from Pext only),
Please check the Trigger Event values in the I2C Controller events…
Hi Shwetanshu,
If you haven't already I recommend watching the tutorial series on how to use the EVM and the GUI tool to configure the PD controller (linked below). You can download the GUI directly through here: https://www.ti.com/tool/TPS6598X-C…
Hi Thomas,
Thank you for reaching out!
1- What is your end-application here? Are you following a reference design or needing to support TBT 4?
2- Here is a link to the latest GUI (v6.1.4) available on TI.com: https://www.ti.com/tool/TPS6598X-CONFIG
Best…