Part Number: TPS65994AD Hi Sir,
My customer is using 994AD at their Alder lake product design. They'll change platform to MTL in new design. Can they use 994AD continuely or have to use 994BH? And any HW setting they have to take care if they have to…
Hi Shubha
I have another question about TPS65994AD FW Setting
Device 1 has two Ports contain Port1 and Port 2,Can I turn off Port2(0x24) separately?
If it's OK ,What are the setup steps?
Part Number: TPS65994AD HI
We are planning to use the pd controller TPS65994ACYBGR. We need the power consumption and power dissipation.
Kindly check and share
Part Number: TPS65994AD Other Parts Discussed in Thread: TPS65994 The customer found when the TPS65994 is as sink:
1: When the input voltage is 5V, the chip power consumption is almost 0W (about 0-0.1W), which is very stable. 2: When the input voltage is…
Part Number: TPS65994AD Other Parts Discussed in Thread: TPS65992DBH , TPD6S300 Hi,
For TPS65992DBH, what is the LDO current ability?
Could we use it to provide TPD6S300 3.3V power?
Thanks!
Jeff
Part Number: TPS65994AD Hi, I'm looking to implement USB 3.1 EPR PD Sink design in my product . I've seen several posts that state that there should be design resources and information by now, but I can't seem to find anything. Any advice?
Part Number: TPS65994AD Other Parts Discussed in Thread: TPS65994BH We are currently using the GUI tool version 6.4.32 to configure the TPS65994BH firmware.
However, I received a .PJT file from someone else and wanted to compare the settings.
The .PJT…
Part Number: TPS65994AD Other Parts Discussed in Thread: TPS66994 Hi AE,
In the TPS66994 spec defined, the address of Port A is 0x20 and Port B is 0x24.
The DBfg (2D 128bit ) has been successfully cleared, After I sent 4CC CMD (08h) to PD in Port A. …