Part Number: TPS709 Tool/software: Hi support team,
I am trying to replace my ABLIC S1222B-30 (SOT-23-5 package) with the TPS70930DBVT. www.ablic.com/.../S1222B_D_E.pdf
However, the pin assignments for pin 3 (EN) and pin 4 (NC) are different. Therefore…
Part Number: TPS709 Tool/software: We kindly request the thermal modeling data and power dissipation characteristics for the component- TPS709. Including clarification on whether its thermal models is of the 2R type or lumped model type.
Part Number: TPS709-Q1 Tool/software: Hello All,
Received some questions for an analysis being done by my customer:
Is there a max leakage current for the enable pin if 3.3V is applied?
Is the +-1% dc accuracy the proper accuracy to be used for…
Part Number: TPS709 Tool/software: When using TPS709, when the output voltage is 3.3V and the output current is Iout=20uA, and the input voltages are 1V/1.5V/2V/3V/3.5V, what are the grounding currents of TPS709
Part Number: TPS709 Tool/software: Here, we are using TI TPS70915DBVR linear voltage regulator to get fixed 1.5 V, which provides the reference voltage for the current sensor LKSR 15-NP. However, we are observing the following scenario.
TI TPS70915DBVR…
Part Number: TPS709 Hello ,
I also have one doubt regarding input capacitance that you have selected 100uF. How you calculated the value for input capacitance ???