Part Number: TPS709-Q1 Other Parts Discussed in Thread: TPS709 As per GMW 3097 for General Motors. it requires the load dump @ 34V Ri 2 ohm 10 pulses 15 seconds apart.
We have 33.7V @400ms applied to the IN pin. The data sheet calls out a max of 32V.
…
Part Number: LM1117 Other Parts Discussed in Thread: LP5912 , TPS709 , TPS7B7701-Q1 , TPS7B4256-Q1 , TL1963A , TPS7A45 , TPS706 Hi team,
Does TI have some feature like this? the integrated back-to-back diode of LDO?
Like the below block. SGM2205.
Due to customer…
Part Number: TPS709-Q1 Hi,
When manufacturing an end-equipment using the following products from a customer,
there was an inquiry about whether it would be a problem in obtaining UL standard certification.
Can there be a problem in obtaining UL standard…
Part Number: TPS709-Q1 Other Parts Discussed in Thread: TPS709 Hello Guys,
Good day.
Our customer re using TPS70933QDBVRQ1 in a space application and cannot leave pins floating due to plasma charging. What equivalent voltage divider can they use on the…
Part Number: TPS709-Q1 Hi,
In the datasheet there is a description of the TPS70950DBVR that the EN-input can float, so I did not connect it to GND or Vout. This is also the case with the TPS70950-Q1, but I can't find a statement in the datasheet if the…
Part Number: TPS709-Q1 Other Parts Discussed in Thread: TPS709 , TPS7B69 , TPS7B69-Q1 Hello Guys,
Good day.
Our customer's PCB design have already been done and mass-produced, but they are having shortage of AP7370-50W5-7 and is looking to TPS70950QDBVRQ1…
Part Number: TPS709-Q1 Off 12V battery application, where the TPS70950-Q1 is considered to provide low Iq supply for a CAN transceiver in a specific mode of operation of <100uA current draw from 12V battery (for whole product).
However, when not in…
Part Number: TPS709-Q1 Dear Sir,
could you let me know value of Plating- Layer thickness (Tolerances), Inner layer- Layer thickness (Tolerances) for TPS70933QDRVRQ1 such as 12μm(±0.2μm).
Thanks.
Part Number: TPS709-Q1 Other Parts Discussed in Thread: TPS709 Hi,
I am using TPS70912QDBVRQ1 IC for converting 18V to 1.2V output. Output load is 10mA worst case.
When I am doing HALT temperature on board. I Observed output voltage is keep increasing…
Part Number: TLV766-Q1 Other Parts Discussed in Thread: TPS709 , TPS7A20 , TPS7A47 , TPS7A24 Hi team,
TLV766-Q1 requires 2mΩ ESR as recommended operating condition.
While, the datasheet also states that "The device is designed to be stable using low…