Part Number: TPS715 Hello,
I'm running my own load transient simulation and it's not turning out very close at all to the datasheet. Can someone advise to why this might be? Am i missing something in my sim? (Attached)
TPS715.TSC
Thanks…
Hello Naveen,
The PSpice model for the TPS715 non Q1 version can also be used, as these devices share the same die and characteristics. We do offer an unencrypted model:
https://www.ti.com/lit/zip/slvmbh3
Please see attached.
2627.Unencrypt.zip
Best, …
Part Number: TPS715 When 12V was input to TPS71550 with no load, the output voltage was not 5V but 10 V or more. Does this device specify a minimum load current?
Part Number: TPS715 Hello,
TPS715 reference seems 1.205V but I couldn't find the reference accuracy information.
Is the accuracy +/-4% which is Vout accuracy?
When we calculate Vout variation, it can calculate from vref and resistor divider min/max…
Part Number: TPS715 Hello guys,
One of my customers is evaluating TPS71530 on their own board for their new products.
In the evaluation, they found that about 0.6V overshoot was happend at powered up.
Their TPS71530 input is connected to 5V linear regulator…
Part Number: TPS715 Our customer ask me about the value of the internal divided resister(R1 and R2) in TPS71525.
Please let me know about two resister value.
Regards,
Tamio
Part Number: TPS715 Hi Team,
I'm using the TPS71501 generate a 5-V output from a 12-V supply and the load current is about 5 mA.
When calculating the resistances of the resistor divider, I found something that contradicts each other.
1. Using the…
Part Number: TPS715 Hi All,
I have a battery application that requires very light loads and the Vout Accuracy of the TPS715 is not specified below 100uA. Do we have any data on Vout Accuracy from 1-10uA? If not ,can you suggest an alternate part? The…
Part Number: TPS715 Hello Team,
My customer intend to use TPS715 for 24V to 5V_20mA, which has power loss 0.38W, since TPS715 is a SC70 package, can you tell if 0.38W for SC70 package is OK? or not recommended? in a case of 25C room temperature, what…
Part Number: TPS715 Support Path: /Product/Production, ordering, and quality/Packaging information/ Hi,
My customer is asking for the UL-Certificate of TPS71525DCKR.
I can't find it online. Is it possible to get it?
Cheers,
Giulliano