Part Number: TPS720
Hi Sir,
My customer would like design Bary trail J1900.
Would you please let us know that TPS72012 is able to support this platform?
BR,
SHH
Part Number: TPS720 Hello,
I would like to confirm VBIAS supply of TPS72018
Is it possible that VBIAS connects to the power supply 3.3V to VIN?
VIN=3.3V (VBIAS=3.3V)
VOUT=1.8V
Thanks,
KM
Part Number: TPS720 Hi,
I have the following 1.8V power supply using the TPS720 (see schematics below):
It provides the MGTVCCAUX power domain for an Xilinx FPGA.
There is nothing on the output power domain except an additional 4.7uF decoupling…
Part Number: TPS720-Q1
Hi TI,
Please find the attached image. It is from TPS72028QDRVRQ1 datasheet. What my question is, why minimal current change huge voltage change is occurred?? ie,) If output current changed to 1mA to 1.7mA means the voltage…
Part Number: TPS720-Q1 Hello,
My customer is using TPS72029 as follows.
Vin =3.3V
Vout = 2.9V
Iout(max) = 100mA.
They also plan to put 5V for VBIAS pin and plan to get the 5V from 12V using a shunt regulator.
But, in order to that, they…
Part Number: TPS720-Q1 Hi Team,
Good day.
My customer is not able to find TPS72009QDRVRQ1 pin1 orientation in the reel for the WSON-6 package.
This is missing in the datasheet, can you help me on this?
Best Regards,
-Renan
Part Number: TPS720 Hi Webmaster,
My customer designed TPS72018DRVR SON package.
But I can't figure out any dimension specification in the datasheet.
Can you share me correct data?
Regards,
David
Part Number: TPS720-Q1 Other Parts Discussed in Thread: LP5907-Q1 , TLV702-Q1 Hi Team,
My customer is looking for an LDO to convert 3.3V to 2.8V for some really sensitive sensors, the 3.3V is bucked down from 12V supply (2.2Mhz switching converter)…
Part Number: TPS720 Hello,
can you please advise the efficiency level of the voltage regulator P/N: TPS72025QDRVRQ1 and if/how the output voltage can be regulated?
Or would there be another high efficiency voltage regulator available with an even…
Part Number: TPS720
I am interested in learning more about TPS720xx in the DSBGA package. What is the reliability comparison for underfill or not underfill?