Part Number: TPS732 Other Parts Discussed in Thread: TINA-TI
Tool/software: TINA-TI or Spice Models
Hi Team, There is "TPS73250 TINA-TI Transient Reference Design" in the following link. http://www.ti.com/product/TPS732/toolssoftware The result…
Part Number: TPS732 My company was designated to review a medical company PCB.
We discovered that the main issue was the TPS73250DBVT, it had 5,5V as input, and had (5,5V-dropout) in the output, it should be a fixed 5V regulator.
This problem happened…
Part Number: TPS732-Q1 Hi, Linear team
Do you have protection function about short to GND and short to battery on the TPS732-Q1?
Thanks
Best Regards
Gerald
Part Number: TPS732 Other Parts Discussed in Thread: TPS736 , Hi Team
My customer Zhuzhou had some questions about TPS732 and TPS736 datasheet:
SBVS037P-“TPS732xx Capacitor-Free, NMOS, 250-mA Low-Dropout Regulator With Reverse Current Protection”…
Part Number: TPS732-Q1 Hello,
I am using the TPS732-Q1 to generate a precision reference. My end equipment has a lot of high powered motors and is polluted with EMI. I am using the adjustable version of TPS732-Q1 to convert 5.5V to 5V @ 150mA. Given that…
Part Number: TPS732-Q1 Other Parts Discussed in Thread: TPS732 Hi All,
There is no SOT-233 information in the TPS732-Q1 data sheet.
http://www.ti.com/lit/ds/symlink/tps732-q1.pdf
Please tell me the information on Pin Configuration and Functions and Thermal…
Part Number: TPS732-Q1 Hello,
One of my customer request the *.stp file for TPS73201QDBVRQ1.
When making PCB library, they want to check interference with 3D data.
I cannot find stp file from TI webpage, so please share the file.
thanks,
TS
Part Number: TPS732-Q1 Other Parts Discussed in Thread: TPS723-Q1 Hello,
I'm looking for 1% accuracy 5V output Q-100 qualified LDO, and found TPS732-Q1 at TI's webpage.
But at page 2 of TPS723-Q1 datasheet, TPS73250-Q1 deleted at 2009.
I think…
Part Number: TPS73201-EP Other Parts Discussed in Thread: TPS732 Dear TI team
TPS732 recommend to use Cout and ESR below 50nCF. I'm gonna use below Capacitor with 10uF and lowest ESR 3.3mohm. but it is not meet requirement below 50nCF.
but I tested…
Hello,
TPS73501DRB requires C FF for the device to remain stable. If C FF cannot be accommodated, then it it cannot be a direct replacement for TPS737. TPS732 is an output adjustable LDO that comes in a 8 pin DRB package and doesn't require CFF for…